HDMI with iMX27

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI with iMX27

883件の閲覧回数
ElwoodFriesen
Contributor I

I'm wondering if anyone has done any HDMI work with the iMX27? I am looking to add HDMI capability (both transmit and receive) to an existing iMX27 design. Some of the challenges are finding IC's that do not support HDCP (we do not need HDCP on the design) and finding devices that interface with 1.8V logic (trying to avoid translation from 3.3V).

 

Does anyone have experience dealing with HDMI and the iMX27? Any HDMI chipset suggestions?

タグ(1)
0 件の賞賛
返信
0 返答(返信)