HDMI to DVI display flickering

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI to DVI display flickering

1,354 Views
sumanthg
Contributor II

I have been working with imx6dq custom board , The  hdmi to dvi display is connected to  hdmi port of imx6 custom board. (based on Sabresd). And booted the board. Now the output of the display is stable. 

If i boot the board and hot plug the hdmi to dvi cable to imx6 board. the output data, which is transmitted from the imx6 board is flickering. with the response of the input events (example: crossing the mouse or typing the data from the 

The display is flickering continuously, how to resolve the problem? 

kernel version : 3.14.52 

android flavor : marshmallow 

0 Kudos
Reply
4 Replies

1,127 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please try with our Android BSP 6.0.1_2.1.0? I tested with both BSP, and no one give me the flickering that you are mentioning.

Best Regards,

Diego.

0 Kudos
Reply

1,127 Views
sumanthg
Contributor II

Hi Diego. 

Can you provide the download link for Android BSP 6.0.1_2.1.0

Regards,

Sumanth

0 Kudos
Reply

1,127 Views
diegoadrian
NXP Employee
NXP Employee

In the below link you can find the download link:

Android OS for i.MX Applications Processors|NXP 

You only need to search for the BSP that you are willing to use.

Best Regards,

Diego

0 Kudos
Reply

1,127 Views
sumanthg
Contributor II

Hi Diego, 

Does hdmi driver support hotplug DVI monitor support ?

Regards,

Sumanth.

0 Kudos
Reply