HDMI support for imx6ul evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI support for imx6ul evk

3,174件の閲覧回数
Shivasagar_myana
Contributor I

Hello, 

        we are trying to enable HDMI support on imx6ul evk, we saw some forums https://community.nxp.com/t5/i-MX-Processors/Enable-HDMI-on-i-MX6UL-EVK/m-p/475912

we found how to populate the HDMI from hardware point view and what drivers we have to enable in the kernel. but we are not able to finding what changes we need to do in the dts and dtsi file. 

we are using yocto souce and imx6ul-14x14-evk.dts and imx6ul.dtsi file i attached the files below.

can any one please suggest what changes need to do in dtsi and dts file.  

0 件の賞賛
返信
4 返答(返信)

3,114件の閲覧回数
Shivasagar_myana
Contributor I

Hi Igor,

Greetings of the Day!!

The hardware changed which were done on the board are mounted U1001, R1002, R1005, R1003, R1007, R1009, R1011, R1010, R1014, D1002, R1004, R1023 and J1001.

From software point of view, we have enabled all the HDMI related  Drivers and modified the dts file as below:

&i2c2 {
clock_frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c2>;
status = "okay";

sii902x: sii902x@39 {
compatible = "SiI,sii902x";
pinctrl-names = "default";
interrupt-parent = <&gpio2>;
interrupts = <13 IRQ_TYPE_EDGE_FALLING>;
mode_str ="1280x720M@60";
bits-per-pixel = <16>;
reg = <0x39>;
status = "okay";

but we are getting error:

sii902x 1-0039: No reset pin found
sii902x 1-0039: Sii902x: cound not find device

and we tested i2c bus  also working, other peripheral addresses are showing but sii902X address is not showing.

could you please help to resolve this problem.

 

0 件の賞賛
返信

3,167件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shivasagar

 

one can look at below knowledge base article

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Install-Debian-8-Jessie-Rootfs-on-NXP-i-...

 

Best regards
igor

0 件の賞賛
返信

3,111件の閲覧回数
Shivasagar_myana
Contributor I

Hi Igor,

Greetings of the Day!!

The hardware changed which were done on the board are mounted U1001, R1002, R1005, R1003, R1007, R1009, R1011, R1010, R1014, D1002, R1004, R1023 and J1001.

From software point of view, we have enabled all the HDMI related  Drivers and modified the dts file as below:

&i2c2 {
clock_frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c2>;
status = "okay";

sii902x: sii902x@39 {
compatible = "SiI,sii902x";
pinctrl-names = "default";
interrupt-parent = <&gpio2>;
interrupts = <13 IRQ_TYPE_EDGE_FALLING>;
mode_str ="1280x720M@60";
bits-per-pixel = <16>;
reg = <0x39>;
status = "okay";

but we are getting error:

sii902x 1-0039: No reset pin found
sii902x 1-0039: Sii902x: cound not find device

and we tested i2c bus  also working, other peripheral addresses are showing but sii902X address is not showing.

could you please help to resolve this problem.

0 件の賞賛
返信

3,096件の閲覧回数
Shivasagar_myana
Contributor I

HI igor,

       could you please let us know is there any update for above issue.

0 件の賞賛
返信