HDMI not working on imx6q sabre auto AI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI not working on imx6q sabre auto AI

2,429件の閲覧回数
suhaskaundinya
Contributor I

Hello,

I am using imx6q sabre auto ai board.

I have just flashed the android oreo images onto an sdcard and tried to boot it to an lvds 10" display and it is working fine.

But when I tried to boot it using HDMI display, there is no output on either the screen or the linux console.

While booting, in the u-boot prompt, I gave the following commands.

=> setenv bootcmd boota mmc1

=> setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0 vmalloc=128M init=/init          video=mxcfb0:dev=hdmi,1280x800M@60,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off       androidboot.hardware=freescale cma=448M galcore.contiguousSize=33554432 androidboot.selinux=permissive

=> saveenv

When I tried to boot the same for dual displays, lvds worked fine but not hdmi.

I connected an adb cable to see the log and I found the follwoing:

01-01 00:11:24.251   290   290 I display : try dev:/dev/dri/card0
01-01 00:11:24.252   290   290 E display : Failed to set atomic cap -1
01-01 00:11:24.252   290   290 I display : entry:fb1 get fb1
01-01 00:11:24.252   290   290 I display : fb1 is overlay device
01-01 00:11:24.252   290   290 I display : entry:fb0 get fb0
01-01 00:11:24.253   290   290 I display : fb0 is hdmi
01-01 00:11:24.253   290   290 I display :  device
01-01 00:11:24.253   290   290 I display : fb0 device plugin
01-01 00:11:24.310   290   290 W display : xres         = 1280 px
01-01 00:11:24.310   290   290 W display : yres         = 720 px
01-01 00:11:24.310   290   290 W display : fps          = 60.00 Hz
01-01 00:11:24.310   290   290 W display : bpp          = 32
01-01 00:11:24.310   290   290 W display : r            =  0:8
01-01 00:11:24.310   290   290 W display : g            =  8:8
01-01 00:11:24.310   290   290 W display : b            = 16:8

I can see that y-resolution is 720 even though I gave 800 in the kernel command line.

Is there any other place from where it might be taking that resolution?

Suggest me on this.

BR,

Suhas R

ラベル(4)
0 件の賞賛
返信
4 返答(返信)

1,967件の閲覧回数
suhaskaundinya
Contributor I

Hello,

I made dual boot work for imx6q sabre auto ai.

The one which is done now is just like screening, If I work on any one of them, the other works simultaneously.

Is there a way wherein I can make them work separately?

BR,

Suhas

0 件の賞賛
返信

1,967件の閲覧回数
suhaskaundinya
Contributor I

Hello Igor,

I have tried that many a times with different resolutions too, but with no luck.

And yes, It is a true HDMI monitor. I have even changed the BoardConfig.mk file to take HDMi instead of lvds by default, yet, it doesn't work.

I changed the ports of HDMI and LVDS in the kernel command line to see the output of HDMI on LVDS display during dual boot, I am getting a distored output with the same resolution given in the kernel command line for HDMI.

The command is as follows:

=>setenv bootcmd boota mmc1
=> setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc3 consoleblank=0 vmalloc=128M init=/init video=mxcfb1:dev=ldb,fbpix=RGB32,bpp=32 video=mxcfb0:dev=hdmi,1280x800M@60,if=RGB24,bpp=32 video=mxcfb2:off video=mxcfb3:off androidboot.hardware=freescale cma=448M galcore.contiguousSize=67108864 androidboot.selinux=permissive

As you can see, I have changed the port numbers. It is taking the same output but with a distorted image.

Nothing on HDMI display, but distorted image with 1280x800 resolution on LVDS.

I am stuck with this from past 3 days.

Could there be any other way from which I can make the HDMI work?

Assist me.

Thanks and BR,

Suhas R

0 件の賞賛
返信

1,967件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Suhas

is it working with "video=mxcfb0:dev=hdmi,1920x1080M@60" as described in

Quick Start Guide. 1280x800 resolution is not a standard CEA-861-D resolution, so the default HDMI driver

doesn't support it. From i.MX6Q documentation hdmi with 1280x800M is not supported (one can try with 1280 x
720) according to Table 33-3. Video Modes i.MX6DQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Also one can try suggestions on

iMX6Q AI board support for 1280×800 HDMI Display 

Best regards
igor

0 件の賞賛
返信

1,965件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Suhas

please try using sect.3.4.2 Booting with single display: HDMI display

attached Android Quick Start Guide. Also check that "true" HDMI monitor was used
with special HDMI cable.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信