HDMI is not detecting in IMX8QM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI is not detecting in IMX8QM

Jump to solution
2,270 Views
vinothkumars
Senior Contributor IV

Dear NXP,

I am working on Android 9 Automotive with IMX8QM. I am using LVDS to HDMI converter to connect between BOARD and Display.

  1. Connector name is not listed under /sys/class/drm:

      ls /sys/class/drm/

         card0 card1 version

     2. dmesg | grep -i HDMI
        console=ttyLP0,115200 earlycon=lpuart32,0x5a060000,115200 androidboot.console=ttyLP0 androidboot.xen_boot=default init=/init consoleblank=0 androidboot.hardware=freescale androidboot.fbTileSupport=enable cma=800M@0x960M-0xe00M galcore.contiguousSize=33554432 androidboot.primary_display=imx-drm firmware_class.path=/ vendor/firmware transparent_hugepage=never video=HDMI-A-2:d androidboot.wificountrycode=CN

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 Kudos
Reply
1 Solution
1,979 Views
vinothkumars
Senior Contributor IV

Hi, 

HDMI is working properly after flash 

"android_p9.0.0_2.1.1-auto-ga_image_8qmek2" this images instead of "android_p9.0.0_2.1.1-auto-ga_image_8qmek".

Regards,

VinothS,

Regards,
Vinothkumar Sekar

View solution in original post

0 Kudos
Reply
3 Replies
1,980 Views
vinothkumars
Senior Contributor IV

Hi, 

HDMI is working properly after flash 

"android_p9.0.0_2.1.1-auto-ga_image_8qmek2" this images instead of "android_p9.0.0_2.1.1-auto-ga_image_8qmek".

Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 Kudos
Reply
1,979 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi VinothS,

I’m afraid that the i.MX8QM is still on preproduction, and you need to contact with your Sales or FAE in case of requiring support.

Additionally, Android Auto is supported under “Commercial Support and Engineering Services” scheme. You could refer to the following link for additional details:

Commercial Support and Engineering Services | NXP 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply
1,979 Views
vinothkumars
Senior Contributor IV

Thank you CarlosCasillas,

Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 Kudos
Reply