Hello,
We found a really strange issue with a MIPI camera and HDMI.
Our MIPI camera works fine, is correctly configured and works with Gstreamer. But if we activate the HDMI ( by inserting the correct vidargs in u-boot : vidargs=video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24;video=mxcfb1:off fbmem=32M) the video "make a roll" when we restart Gstreamer.
This issue only happens when the HDMI is enabled in u-boot.
Another strange issue: when we disabled mxcfb* in the device tree:
&mxcfb1 {
status = "disabled";
};
&mxcfb2 {
status = "disabled";
};
&mxcfb3 {
status = "disabled";
};
&mxcfb4 {
status = "disabled";
};The MIPI does not work at all, the MIPI_CSI_PHY_STATE is constantly equals to 0x200
Any thoughts about this issue? Is it clock related?
We are working on iMX6Q POP package, the MIPI is running at 648MHz.
The image is build by Yocto Pyro, kernel is 4.1.15.
Regards,
Pierre-Olivier
Update:
After my response on the clocks (with or without HDMI), I did some other tests.
My configuration is as follow:
IPU1_CSI0 and IPU1_CSI1 are used by a MIPI source (on virtual channel 0 and 1)
IPU2_CSI1 is used by a parallel camera in BT656.
IPU2_CSI0 is unused
Everything is working, excepted the video scroll.
I get these messages when the video is scrolling, the scroll stops when the video bottom hit the bottom of the screen.
[ 4118.492325] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000001
The message is sent multiple times during the scroll
At the begining of my test, my configuration is:
What I tried:
Any thoughts? Any advices on something I am doing wrong?
Hi Pierre-Olivier
what bsp and gstreamer used in the case. One can try with nxp official
demo images from
Board Support Packages (3)
Demo Images - QWKS Board based on SCM-i.MX 6D/Q
Quick Start Board for SCM-i.MX 6DQ|NXP
Yocto BSP for SCM-i.MX L4.1.15-2.0.0_ga
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for the answer.
It is quite complicated to test the official Yocto BSP, we have to port all our modifications.
We use the Variscite BSP (with some little customisations), with Yocto Pyro, with Gstreamer 1.10.4.
But I have something interesting, the clocks are not the same with or without the HDMI enabled in uboot:
When I disable hdmi via uboot:
This is the two gists with the complete clock summary
My question:
As I understand the iMX6, the IPUx DI are used for display ports/VGA, so why the ipu1_di clock is used (enable_cnt=1) if I only use HDMI?
Regards,