HDMI drive strength control and where can download HDMi firmware files to test?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI drive strength control and where can download HDMi firmware files to test?

1,130 Views
kuda
Contributor II

Hi,

         We are facing issues with HDMI port during EMI test. We fine this link had the same issue.

HDMI drive strength control and pixel clock change - NXP Community

         where can download HDMI firmware files to test?

                                                                      kuda

0 Kudos
6 Replies

1,123 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kuda

 

>where can download HDMI firmware files to test?

 

https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.12.bin

 

HDMI firmware.jpg

 

Best regards
igor

0 Kudos

1,115 Views
kuda
Contributor II

HI!

                Tks for reply quickly.

          Our SOM is the coral board, which linux kenel version is 4.14.98.

           Your link address is for 5.10. Is the firmware is compatible?

           And this firmware is set to decrease drive strength ?

                                                                         kuda

 

 

0 Kudos

1,102 Views
igorpadykov
NXP Employee
NXP Employee

you can find firmware version from Release Notes below for each BSP release

use https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-x.y.bin for download

 

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos

1,079 Views
kuda
Contributor II

HI!

      We follow your example address and check i.MX Linux® Release Notes, Rev. L4.14.98-2.0.0_ga, 05/2019. We can download firmware-imx-8.1.bin successfully.

        But we can't find any notes about HDMI  firmware version control and HDMI drive strength control information.

      How to check hdmi firmware version? We need HDMI lower drive strength to test and pass radio emission verification.

   TKS.

                                  kuda

Tags (1)
0 Kudos

1,057 Views
kuda
Contributor II

HI!

But we can't find any notes about HDMI firmware version control and HDMI drive strength control information.

How to check hdmi firmware version? We need HDMI lower drive strength to test and pass radio emission verification.

We can download firmware-imx-8.x.bin files and try to replace original firmware file then re-flash imx8 image. But we can't find any difference about HDMI drive strength.

 Can someone can help us to control HDMI drive strength ?

tks.                                  kuda

0 Kudos

1,054 Views
igorpadykov
NXP Employee
NXP Employee

for hdmi drive strength one can try settings in

sect.15.5.3.10.2.380 HDP Lane Configuration register (lane0_phy_hdp_tx_ctl - lane3_
phy_hdp_tx_ctl)    i.MX 8QuadMax Applications Processor Reference Manual

 

phy_hdp_tx_ctl_1_0 Tx De-emphasis:

Level 0 ( 0.0dB) results in larger voltage swings
Level 1 (-3.5dB)
Level 2 (-6.0dB) results in smaller voltage swings

phy_hdp_tx_ctl_5_4 Tx Voltage Swing:

Level 0 (400 mV) results in smaller voltage swing
Level 1 (500 mV)
Level 2 (600 mV) results in larger voltage swings

 

Best regards
igor

0 Kudos