HDMI doesn't react on Solo and QP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI doesn't react on Solo and QP

644件の閲覧回数
nexy_sm
Contributor II

Hi all,

I have an issue with HDMI on custom boards, one with Solo and another with Quad.

On Solo board reading any register from HDMI transmitter returns 0s.

On Quad board reading HDMI transmitter registers return correct value.

In both cases there is no output on HDMI. Hot plug signal is present and correct, 0.8 V when no cable is present, and 2.55 V when cable is plugged. Unfortunately I cannot see any clock nor data with the scope. When cable is plugged simply nothing happens.

The U-Boot code we are using to test HDMI works on SABRE AUTO.

Does anybody have any suggestion where to seek for the problem? It is really strange to read 0s from Solo's HDMI transmitter. Also when I want to read Identification register 0s come out.

Thanx and cheers

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

521件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nemanja

SABRE AUTO image may not work for other processors/configurations.

Please choose correct configuration using sect.5.1 Build configurations attached Yocto Guide

for i.MX6Solo and i.MX6QP and build separate images for each processor,

use nxp uboot

uboot-imx.git - Freescale i.MX u-boot Tree 

More documentation can be found on

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信