HDMI does not working on iMX8mq-evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI does not working on iMX8mq-evk

4,624 Views
trongthinh
Contributor IV

I got this error after connecting HDMI cable to iMX8MQ-evk

[ 453.501881] [drm] HDMI/DP Cable Plug Out
[ 453.749877] [drm] HDMI/DP Cable Plug In
[ 454.433798] [drm] HDMI/DP Cable Plug Out
[ 454.681840] [drm] HDMI/DP Cable Plug In
[ 456.965766] [drm] HDMI/DP Cable Plug Out
[ 457.213747] [drm] HDMI/DP Cable Plug In
[ 459.517614] [drm] HDMI/DP Cable Plug Out
[ 459.765664] [drm] HDMI/DP Cable Plug In

My screen resolution is 1024x768. Does current release "Linux 4.9.88_2.0.0 [Current Release]" only support screen with resolution 1920x1080? is it possible to add a new resolution to driver?

 

Tags (2)
12 Replies

2,855 Views
94393400
Contributor III

Hi Thinh Nguyen 

     Do you have resloved this problem?  How to fix ?

2,855 Views
trongthinh
Contributor IV

The driver shows that 65Mhz clock is not supported so I change monitor to 125MHZ clock.

0 Kudos

2,855 Views
joanxie
NXP TechSupport
NXP TechSupport

current bsp shouldn't support this resolution, if you need to add new resolution, you can refer to the patch for imx6 as below:

https://community.nxp.com/message/875581 

2,855 Views
trongthinh
Contributor IV

This patch does not help because driver for iMX8 using drm and dcss instead of mxcfb (iMX6). I found that my screen pixel clock is 65 MHz which is not supported by current driver 

 

[ 2094.460881] [drm] mode:1024x768p60, pixel clock 65000 kHz
[ 2094.466483] [drm] format: 1. REF VAL: YCBCR_4_2_2: 4 YCBCR_4_2_0: 8
[ 2094.472879] [drm] bit per pixel: 8
[ 2094.476460] [drm] Pixel clock frequency: 65000 kHz, character clock frequency: 65000, color depth is 8-bit, pixel clock from PHY: 1.
[ 2094.488501] [drm:phy_cfg_t28hpc] *ERROR* This pixel clock frequency (65000 kHz) is not supported.
[ 2094.497547] [drm:hdmi_phy_init_t28hpc] *ERROR* failed to set phy pclock
[ 2094.504287] [drm:imx_hdp_bridge_mode_set] *ERROR* Failed to initialise HDP PHY
[ 2094.511714] [drm] OPIPE_CFG: gamut = 1, nl = 1, pr = 1, pix_format = 875713089
[ 2095.043816] [drm] HDMI/DP Cable Plug In
[ 2096.749110] [drm] HDMI/DP Cable Plug Out
[ 2097.004782] [drm] mode:1024x768p60, pixel clock 65000 kHz
[ 2097.010379] [drm] format: 1. REF VAL: YCBCR_4_2_2: 4 YCBCR_4_2_0: 8
[ 2097.016782] [drm] bit per pixel: 8
[ 2097.020364] [drm] Pixel clock frequency: 65000 kHz, character clock frequency: 65000, color depth is 8-bit, pixel clock from PHY: 1.
[ 2097.032402] [drm:phy_cfg_t28hpc] *ERROR* This pixel clock frequency (65000 kHz) is not supported.
[ 2097.041449] [drm:hdmi_phy_init_t28hpc] *ERROR* failed to set phy pclock
[ 2097.048186] [drm:imx_hdp_bridge_mode_set] *ERROR* Failed to initialise HDP PHY
[ 2097.055540] [drm] OPIPE_CFG: gamut = 1, nl = 1, pr = 1, pix_format = 875713089

 

 

This is supported clock list: 27MHz, 74.25MHz, 99MHz, 148.5MHz, 198MHz, 297MHz, 594MHz. Any help for porting driver to support pixel clock 65Mhz is welcome.

0 Kudos

2,855 Views
joanxie
NXP TechSupport
NXP TechSupport

for your resolution, you need add in the driver(drivers\video\mxc\mxc_hdmi.c), then you can add your own pixel clock in the structure, for example:

+static const struct fb_videomode wvga_mode = {

+ /* 1280x960 @ 60 Hz */

+ NULL, 60, 1280, 960, 9259, 312, 96, 36, 1, 112, 3,

+ FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,

+ FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_4_3, FB_MODE_IS_VESA,

+};

0 Kudos

2,855 Views
trongthinh
Contributor IV

Thanks for replying me! Can you explain about pixel clock declaration in the structure? 

 

static const struct fb_videomode wvga_mode = {

      /* 1280x960 @ 60 Hz */

      NULL, 60, 1280, 960, 9259, 312, 96, 36, 1, 112, 3,

      FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,

      FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_4_3, FB_MODE_IS_VESA,

};

I confuse with the bold line. What does these numbers mean?

0 Kudos

2,855 Views
joanxie
NXP TechSupport
NXP TechSupport

struct fb_videomode {
const char *name;/* optional */
u32 refresh;/* optional */
u32 xres;
u32 yres;
u32 pixclock;
u32 left_margin;
u32 right_margin;
u32 upper_margin;
u32 lower_margin;
u32 hsync_len;
u32 vsync_len;
u32 sync;
u32 vmode;
u32 flag;
};

2,855 Views
trongthinh
Contributor IV

Thanks for your information. Though it useful, the file you mention "drivers\video\mxc\mxc_hdmi.c" is work with iMX6 and it was not build when i use iMX8. I try luck by modifying "drivers/gpu/drm/hdp/imx-hdp.c", yet I still got the issue. I am sure that this is the correct file I need to modify. Unfortunately, The issue still there. Any hint, suggestion is welcome.

 

0 Kudos

2,855 Views
joanxie
NXP TechSupport
NXP TechSupport

did you try to modify the drive source code "imx-hdmi.c" under the drivers/gpu/drm/imx/hdp? my laptop don't have source code to check for you, pls check this file

0 Kudos

2,855 Views
trongthinh
Contributor IV

I have just checked the file (imx-hdmi.c). I also attached it. I think no suitable line to apply the patch. I think this clock (65Mhz) is get when driver reads information from edid. It is not hard code.

0 Kudos

2,855 Views
nagashree_vm03
Contributor I

Thinh Nguyen

Did you find the solution for this issue ?

0 Kudos

2,855 Views
trongthinh
Contributor IV

no! just a workaround by changing monitor clock to 125MHz

0 Kudos