Hi
I have been porting linux BSP 3.10.17_1.0.2 BSP (Yocto) for our custom board based on i.MX SDP and using i.MX6DL.
We do not have lvds display on our board (we have only HDMI), not charger, no camera, no GPIO buttons, no audio codec, no ethernet.
So, in the DT files, I have removed all those HW configuration.
The linux boots up, I can see from the debug uart. However, no display on HDMI. the boot argument was set as below (Hdmi on fb0)
setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 video=mxcfb1:off - does not work, no output to HDMI display
When I tried to set HDMI to fb1, then i can see the display only when the linux is fully booted up, i.e. I do not see the yocto progress bar.
setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} video=mxcfb0:off video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24 – works only if mxcfb0 is set to off
Did anyone have similar issue? Any suggestion? I am not very familiar with DT files and so, not sure if there is any dependent code I might removed because i am also having issue with USB H1 (USB H1 not working properly on iMX6DL custom board), but still not solved yet.
Thanks and regards,
Paramod
Hi,
I ask for some help on review on DT files but it seems it is paid support from Freescale. I get this from FAE instead. But before going for any paid support, if anyone can help, it will be much appreciated.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=LINUX-ANDROID-COMMERCIAL-SUPPORT
Thanks in advance,
Paramod
Hi Paramod,
You could try the following workaround for enabling the HDMI display from the beginning. On the U-Boot command line:
editenv mmcargs
Add the following to the end of the mmcargs variable:
video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
saveenv
boot
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Paramod,
Have you ensured that you added the mentioned command at the end of the mmcargs values instead of deleting something? It should be as following after the modifications:
setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
Hope this will be useful for you.
Best regards!
/Carlos
Hi Paramod,
Did you applied the modifications over an image that you previously tried to modify? I tested the mentioned method and worked properly without hanging the boot.
Maybe a good idea could be flashing again the image on your board and just apply the mentioned configuration.
Hope this will be useful for you.
Best regards!
/Carlos