HDMI Tx without DCSS in IMX8MQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI Tx without DCSS in IMX8MQ

937 Views
jemish_1990
Contributor IV

We are going to make product based on IMX8MQ (MIMX8MQ6DVAJZAA) processor.  Currently we are doing POC on IMX8MQ processor EVK.

  • Based Technical Reference manual and sample device tree files what I see that we are always using DCSS controller to drive output on HDMI screen. Is there any way we can use HDMI TX directly without using DCSS controller?
  • Basically we want to use MIPI DSI interface for DSI panel and use DCSS controller for different features (scaling, rotation, overlay etc).
  • And use HDMI display as it is.

Is what I describe here is possible in IMX8MQ?

Thanks,

Jemish

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

717 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, the DCSS is crucial for the HDMI output on the i.MX8MQ. You cannot have the HDMI output without the use of the DCSS. I apologize for the inconveniences this could give you.

Best regards,

Diego.

0 Kudos
Reply

717 Views
jemish_1990
Contributor IV

Thanks Diego !

It is clear now.

You can mark this discussion as close.

0 Kudos
Reply