HDMI OUT Driver probe successes but Video is not coming in IMX8 platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI OUT Driver probe successes but Video is not coming in IMX8 platform

1,334 Views
vinothkumars
Senior Contributor IV

Hi,

 

Video is not working with IMX8 variant,

But interrupt is getting while connect and disconnect the cable

[ 1.950871] imx-drm display-subsystem: bound 56268000.hdmi (ops imx_hdp_imx_ops)
[ 53.541726] imx-drm display-subsystem: HDMI-A-1: EDID is invalid:
[ 53.601575] i.mx8-hdp 56268000.hdmi: failed to get edid, use default video modes
[ 53.609715] i.mx8-hdp 56268000.hdmi: No EDID function, use default video mode
[ 53.617390] [drm] HDMI/DP Cable Plug In
[ 72.984430] [drm] HDMI/DP Cable Plug Out
[ 73.800544] i.mx8-hdp 56268000.hdmi: No EDID function, use default video mode
[ 73.807977] i.mx8-hdp 56268000.hdmi: No EDID function, use default video mode
[ 73.823163] [drm] HDMI/DP Cable Plug In

 

Regards,
Vinothkumar Sekar
0 Kudos
Reply
2 Replies

1,323 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

from log "hdmi: failed to get edid" seems there is no signal on hdmi i2c :

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.d...

 

1.jpg

one can try to check HDMI SCL,SDA signals with oscilloscope and debug it using

hdmi driver sources described in sect.6.4.6.7.3 Source Code Structure   i.MX Linux Reference Manual​

 

Best regards
igor

0 Kudos
Reply

1,288 Views
vinothkumars
Senior Contributor IV

Thank you Igor for the reply.

Regards,
Vinothkumar Sekar
0 Kudos
Reply