HDMI_HPD signal for i.MX 8M Plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI_HPD signal for i.MX 8M Plus

435 Views
borisberman
Contributor III

Hello to all,

What is the max. voltage on HDMI_HPD signal for i.MX 8M Plus?

The power group for it (NVCC_ECSP1_HDMI) is connected to 3.3V, we only use this pin as a hot plug detect input.

In other words, does this input the +5V tolerant in the i.MX 8M Plus?

 

Thank You,
Boris

0 Kudos
2 Replies

431 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the imx8mp hardware design guide:

"3.9 HDMI connectivity
The i.MX 8M Plus provides an HDMI transmitter capable of supporting an HDMI2.0 compatible output. Level shifters are required on HDMI_DDC_SCL, HDMI_DDC_SDA, HDMI_HPD, HDMI_CEC signals to shift the original 3.3V or 1.8V level to 5V required by HDMI interface."

0 Kudos

426 Views
borisberman
Contributor III

Hello Joan,

Thanks a lot for your reply.

Boris

0 Kudos