HDMI Error on I.MX6Q SDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI Error on I.MX6Q SDB

ソリューションへジャンプ
3,291件の閲覧回数
ArcheeW
Contributor I

Hi,

   I run android4 on mx6q sdb.

   the BSP : imx-android-r13.4-ga, and patch use :r13.4-ga_sdb_sdp;

 

  After I set up u-boot cmd as :

    setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 vmalloc=400M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60 video=mxcfb1:off video=mxcfb2:off fbmem=28M

 

   and saveenv ; reset the board.  When I plug the HDMI to VGA connector, the debug serial output:

/////////////////////////////////////////////////////////

  fbcvt: 1920x1080@60: CVT Name - 2.073M9

mxc_hdmi mxc_hdmi: same edid

.........

mxc_hdmi mxc_hdmi: same edid

////////////////////////////////////////////////////////

But, the HDMI Monitor show nothing.

 

Is someone know why!?

 

Thanks!

 

 

 

 




 


Original Attachment has been moved to: debug.txt.zip

ラベル(3)
タグ(1)
0 件の賞賛
1 解決策
964件の閲覧回数
hemalgandhi
Contributor III

Hi,

After reviewing attached log, it looks that android is booted successfully. If you are using HDMI to VGA connector, you need to set input signal as VGA from your Display unit.

If your display supports HDMI input directly, you can try to connect board with Display unit using HDMI to HDMI cable and adjust input signal as HDMI from  your display unit.



Thanks,

Hemal

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
964件の閲覧回数
hoangduong
Contributor II

Hi ArcheeWoo,

At this moment, i have same problem. I set up uboot cmd as you did and i see the kernel message show

fbcvt: 1920x1080@60: CVT Name - 2.073M9

but when android boot up, i can not see anything on HDMI monitor, i also went to display advanced options on android settings but HDMI settings not there. I also use a HDMI to VGA cable.

did you resolve this problem?

Thanks.

0 件の賞賛
964件の閲覧回数
fabiof
Contributor IV

Hi

I currently have the same problem too, some news about possible fix?

Thank you

0 件の賞賛
965件の閲覧回数
hemalgandhi
Contributor III

Hi,

After reviewing attached log, it looks that android is booted successfully. If you are using HDMI to VGA connector, you need to set input signal as VGA from your Display unit.

If your display supports HDMI input directly, you can try to connect board with Display unit using HDMI to HDMI cable and adjust input signal as HDMI from  your display unit.



Thanks,

Hemal

0 件の賞賛