HD video 720p and 1080p slow motion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HD video 720p and 1080p slow motion

6,696 Views
joylin
Contributor II

Hi All,

The browser cannot play youtube HD video.

Browser play youtube 720p video like playing in slow-motion till the end of video on imx6q-sabresd with android5.1.1 Linux 3.14.52.The cpu usage is 85%~100%. The Chrome v54.0.2840.68 play 720p and 1080p  slowly, too.

The option of Browser in AndroidManifest.xml android:hardwareAccelerated = true already.
Browser playing vimeo 720p video is good.
The 720p video from SD-card plays well and the cpu usage is less than 20%.

What problem of browser playing HD video?
Any suggestion for improve playing youtube HD video by Browser are very welcome.

Thanks!

Joy

Labels (4)
0 Kudos
1 Reply

5,655 Views
b36401
NXP Employee
NXP Employee

Please refer this discussion regarding to hardware video acceleration in web browser:
https://community.nxp.com/thread/302210

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos