HAB4 Version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HAB4 Version

2,091 Views
michael_glembot
Contributor IV

Hello,

is there a list of which HAB4 version runs on which ROM SOC? Or does the HAB Version even differ in their SOC revisions? Then I would need at least the revision from the first HW release. Can you help me out? Have I forgotten any other SOCs using HAB4?

SOCHAB Version
imx6ulz?
imx6ull?
imx6UltraLite?
imx6sll?
imx6SoloLite?
imx6SoloX?
imx6Solo/DualLite?
imx6Dial/Quad?
imx6DualPlus/QuadPlus?
imx8m Mini?
imx8m Nano?
imx8m Plus4.5
.. 
0 Kudos
Reply
2 Replies

440 Views
petterm
Contributor I

A follow-up question to above table. I guess that is for latest silicon revision, meaning 1.4 for imx6SoloX for example?

I tried to check the hab_version in u-boot and I get (below board run silicon revision 1.4):

=> hab_version
HAB version: 4.2

I want to check different silicon revisions if they have boot rom fixes for below issues included or not

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-Vybrid-Security-Vulnerability-Errat...

How can I check that in the best way? From my understanding silicon revision 1.4 should(?) be safe, but also that is a bit unclear how I can verify and read more about.

0 Kudos
Reply

2,086 Views
joanxie
NXP TechSupport
NXP TechSupport

I fill in the table, in fact the HAB version depends on the different silicon revision, I updated on the latest version

SOC HAB Version
imx6ulz HAB 4.2.6
imx6ull HAB 4.2.6
imx6UltraLite HAB 4.2.6
imx6sll HAB 4.2.6
imx6SoloLite HAB 4.2.7
imx6SoloX HAB 4.2.7
imx6Solo/DualLite HAB 4.2.7
imx6Dial/Quad HAB 4.2.7
imx6DualPlus/QuadPlus HAB 4.2.7
imx8m Mini HAB 4.3.9
imx8m Nano HAB 4.5.2
imx8m Plus HAB 4.5.6
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----