Hi freescale team,
Thanks for your fast reply.I followed your instructions and i am
not getting any HAB events.Now i fused HW_OCOTP_SRK(0-7) with fuse bianary
values.
Now my *hab_status *command not giving HAB events . In your
previous reply you told that make *SEC_CONFIG *to closed only after
checking all hab functions.
Now can you suggest me how to check HAB functions from
u-boot.In my u-boot i have only *hab_status *is available regarding HAB
check.
Checking hab_status is enough?
Do i need to check anything else before making SECURE_CONFIG to closed?
If yes please help me to check HAB functionality?
Thank You
With Warm Regards,
Sai Suryanarayan S
*Cell : *+91 8867185975 | Skype : Suryanarayan sarabu
Please use section 6.1 (Error Logging) of AN4581 (Secure Boot on i.MX50, i.MX53, and
i.MX 6 Series using HABv4 ). In particular, please pay attention on the example, which
"can be modified to also report all warning events, by using HAB_STS_ANY inhab_rvt_report_event,
instead of HAB_FAILURE".
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------