Hi Community,
Here are my environment details, i.MX6Quad 1GB module, Kernel: 4.9, Uboot: 2019.07.
I am trying to get Secure boot. I am following documents like AN4581 and High Assurance Boot (HAB) for dummies .
Here is a procedure which I follow,
A) Compiled Uboot with CONFIG_SECURE_BOOT enable. and make V=1.
B) Run hab4_pki_tree.sh in Code Signing Tool release version 3.1.0.
$ ./hab4_pki_tree.sh
$ ../linux64/srktool -h 4 -t SRK_1_2_3_4_table.bin -e SRK_1_2_3_4_fuse.bin -d sha256 -c \
./SRK1_sha256_4096_65537_v3_ca_crt.pem,./SRK2_sha256_4096_65537_v3_ca_crt.pem,./SRK3_sha256_4096_65537_v3_ca_crt.pem,./SRK4_sha256_4096_65537_v3_ca_crt.pem -f 1
$ hexdump -e '/4 "0x"' -e '/4 "%X""\n"' < SRK_1_2_3_4_fuse.bin
0x94153933
.
.
.
.
.
.
0xXXXX90
C) Generate CSF binaries for SPL and u-boot-ivt.img as below. For CSF file see the attachment.
$ ./cst --o csf-SPL.bin --i csf-uboot-SPL
CSF Processed successfully and signed data available in csf-SPL.bin
$ ./cst --o csf-uboot-ivt.bin --i csf-uboot-ivt
"CSF Processed successfully and signed data available in csf-uboot-ivt.bin
D) Concat both CSF binaries.
$ cat u-boot-ivt.img csf-uboot-ivt.bin > u-boot-ivt_signed.img
$ cat SPL csf-SPL.bin > SPL_signed
E) Flashed SPL_signed and u-boot-ivt_signed.img in module.
F) Programmed the fuse in Uboot with fuse command.
-> fuse prog -y 3 0 0x94153933 (similar for other banks also with respected values.)
Now I checked hab_status and I got as below,
-> hab_status
Secure boot disabled
HAB Configuration: 0xf0, HAB State: 0x66
No HAB Events Found!
Still, I didn't close the device. Because I have below doubts related to that,
1. Which binary should I sign?
I am getting executables like u-boot-dtb.img , u-boot-ivt.img, SPL . I am confused which to sign.
2. Can I use directly the concatenated image(SPL_signed) as below?
$ ./cst --o csf-SPL.bin --i csf-uboot-SPL
$ cat SPL csf-SPL.bin > SPL_signed
In some documents, to align the image they are filling junk value with objcopy command. Whether it is required here also?
3. How can I confirm whether I did all steps correctly or not?
4. Is it mandatory to use signed Kernel image ? Can I use only signed Uboot alone?
5. How to sign the Uboot for imx_usb_loader?
Thanks in advance
Regards,
Deven