HAB Boot Signed Kernel issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HAB Boot Signed Kernel issue

1,145 次查看
jones_chang
Contributor II

Hi NXP Pals,

I try to enable secure boot but I meet following condition,

HAB Boot Signed Kernel: HAB Events 

any update to fix it??

Please help to check following info:

=> hab_status

Secure boot enabled

HAB Configuration: 0xcc, HAB State: 0x99
No HAB Events Found!

=> hab_auth_img 0x12000000 0x68c020

Authenticate image from DDR location 0x12000000...

Secure boot enabled

HAB Configuration: 0xcc, HAB State: 0x99

--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x08 0x41 0x33 0x05 0x0a 0x00

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_IVT (0x05)
CTX = HAB_CTX_AUTHENTICATE (0x0A)
ENG = HAB_ENG_ANY (0x00)

0 项奖励
回复
1 回复

1,062 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jones

one can try with latest "Code Signing Tools" available on

i.MX Software and Development Tools | NXP 

use uboot hab examples and guidelines on

habv4\imx\doc - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复