H.265 decode,using gstreamer pipeline on IMX8M mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

H.265 decode,using gstreamer pipeline on IMX8M mini

3,328 Views
wangliu
Contributor I

Hi,

I am using gstreamer pipeline to decode H.265 video on imx8m mini board, but I have some problem as follow:

gstreamer pipeline:

gst-launch-1.0 -v filesrc location=h265_720p.265 ! qtdemux ! h265parse ! queue ! vpudec ! glimagesink async=false enable-last-sample=false qos=false sync=false

issue on the Linux shell:

root@imx8mmevk:/unit_tests/Audio#
root@imx8mmevk:/unit_tests/Audio#
root@imx8mmevk:/unit_tests/Audio# gst-launch-1.0 -v filesrc location=h265_720p.265 ! qtdemux ! h265parse ! queue ! vpudec ! glimagesink async=false enable-last-sample=false qos=false sync=false
Setting pipeline to PAUSED ...
====== VPUDEC: 4.4.4 build on May 6 2019 06:48:28. ======
wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Apr 24 2019 05:16:41)
vpulib: 1.1.1
firmware: 1.1.1.0
Pipeline is PREROLLED ...
Got context from element 'sink': gst.gl.GLDisplay=context, gst.gl.GLDisplay=(GstGLDisplay)"\(GstGLDisplayWayland\)\ gldisplaywayland0";
ERROR: from element /GstPipeline:pipeline0/GstQTDemux:qtdemux0: This file is invalid and cannot be played.
Additional debug info:
../../../git/gst/isomp4/qtdemux.c(750): gst_qtdemux_pull_atom (): /GstPipeline:pipeline0/GstQTDemux:qtdemux0:
atom has bogus size 18446464110561329920
ERROR: pipeline doesn't want to preroll.
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Freeing pipeline ...

Could you help me to fix this bug? Thanks.

Labels (1)
0 Kudos
Reply
2 Replies

2,678 Views
wangliu
Contributor I

My software version is:     4.14.78-imx_4.14.78_1.0.0_ga+g94da7bd   imx8mmevk.

0 Kudos
Reply

2,678 Views
joanxie
NXP TechSupport
NXP TechSupport

could you play the video by "gplay-1.0 h265_720p.265" or "gst-launch-1.0 uri=file:///h265_720p.265"?

0 Kudos
Reply