Hello,
I'm using a IMX6 solo based platform. My kernel version is 3.10.17 and Gstreamer1.0 is used. I used gplay1.0 as well as gst-launch-1.0 playbin uri=file:///<file name>
However when I play a video file (stream type : h264) I'm getting a SIGSEGV with the following error log:
====== AIUR: 4.0.2 build on Mar 30 2015 13:08:02. ======
Core: MPEG4PARSER_06.07.04 build on Dec 5 2013 11:47:49
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm11_elinux.so.3.2
Caught SIGSEGV
Spinning. Please run 'gdb gst-launch-1.0 277' to continue debugging, Ctrl-C to quit, or Ctrl-\ to dump core.
What can be the issue ?
Thanks,
Chaitanya Dhere