We are having Nitrogen 6 max board , connected with OV5640MPIP camera, and we are able to capture display and view the capture data on same nitrogen device in Linux platform.
Now we need to stream display capture from Nitrogen 6max board to PC and other imx6 board using gstreamer.
Can you please suggest the gst command and pipeline configure value to stream display capture data over RSTP/UDP Sink/Source from imx board to pc and one imx board to other imx board.
I have tried the below command but after capture data on file i am not able to play the video
on server
gst-launch-1.0 imxv4l2videosrc device=/dev/video1 ! queue ! rndbuffersize max=1316 min=1316 ! udpsink host=192.168.2.102 port=1234 sync=false
on receiver
gst-launch-1.0 udpsrc port=1234 ! filesink location=check.mp4
Please suggest the right command
Thank you !!! :smileyhappy:
Thank you for you support
we achieve gstreamer through
gst-launch-1.0 imxv4l2videosrc device=/dev/video1 ! imxvpuenc_h264 ! rtph264pay ! queue ! rndbuffersize max=1316 min=1316 ! udpsink host=your_ip port=1234 sync=false
Thank you
Hi niket,
why don you try
linux side:
gst-launch-1.0 mfw_v4lsrc device=/dev/video1 fps-n=30 ! vpuenc codec=6 ! queue ! rtph264pay ! udpsink host=yourip port=5000 –v
pc side:
open the attached H264.sdp file using VLC. Then you can find the picture from camera on mx6 board, pls don’t forget to load camera module