Gstreamer plugin to have reduced latency in streaming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gstreamer plugin to have reduced latency in streaming

1,240件の閲覧回数
snehal_jadhav
Contributor III

Hi,

We are streaming camera from imx6q platform on remote display which has NVIDIA GPU. We are using below gstreamer pipeline on remote display to stream camera. In below pipeline we are using NVIDIA decoder plugin.

gst-launch-1.0 -e -v udpsrc port=5000 ! application/x-rtp,encoding-name=H264,payload=96 ! rtpjitterbuffer latency=0 drop-on-latency=TRUE ! rtph264depay ! video/x-h264 ! h264parse ! nvdec ! glimagesink sync=false

with this pipeline we are getting ~116ms to ~175ms latency in camera streaming on remote display. How we can reduce our latency in video streaming. Is there any gstreamer plugin which can help us reduce latency or any other way.

Thanks

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

924件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi,

I am exploring the issue, and below are the details required for further analysis to debug this issue. Can you please help me with the same?

  1. Can you please provide me with the command which you are firing at the processor side?
  2. Through which medium the camera data is sent to the remote display?

 

Best Regards,

Dhruvit.

0 件の賞賛
返信