Gstreamer library not working on imx8mm evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gstreamer library not working on imx8mm evk

1,135 Views
TBYE
Contributor I

I am using imx8m evk with imx-image-core, in which while fetching feed from camera getting internal stream error from gstreamer.

Attached are the result gst-device-monitor and gst-inpect-1.0.gst-device-monitor.JPGgst-inspect-1.0-output.JPG

0 Kudos
Reply
5 Replies

1,089 Views
TBYE
Contributor I

Erza_0-1615980446045.png

Adding packagegroup-fsl-gstreamer1.0 in imx-image-core.bb file resolves the gstreamer issue.

0 Kudos
Reply

1,113 Views
TBYE
Contributor I

I am using imx-image-core , kernel 5.4.24 built using instruction provided by imx- yocto guide. It is working fine with imx-image-full.

Erza_0-1615264965849.png

 

0 Kudos
Reply

1,105 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

1,119 Views
TBYE
Contributor I

 

 

0 Kudos
Reply

1,127 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erza

 

what bsp used in the case, one can try Demo Image  i.MX 8M Mini EVK

use Chapter 7 Multimedia   i.MX Linux User’s Guide​

 

Best regards
igor

0 Kudos
Reply