Gstreamer Build error : Yocto imx6sl

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gstreamer Build error : Yocto imx6sl

3,436件の閲覧回数
karthikeyanraju
Contributor III

Hi,

Building Yocto version 4.9.88.

$bitbake fsl-image-qt5-validation-imx

branch=MM_04.03.05_1804_L4.9.88_MX7ULP_GA, attempting MIRRORS if available
ERROR: gstreamer1.0-plugins-base-1.12.2-r0 do_fetch: Fetcher failure: Fetch command export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-A5I09GC0ro"; export SSH_AUTH_SOCK="/run/user/1000/keyring-ixoOhL/ssh"; export PATH="/home/zumi/Project/Yocto_4_9_88/nxp-yocto/bld-xwayland/tmp/work/imx6slevk-poky-linux-gnueabi/gstreamer1.0-plugins-base/1.12.2-r0/recipe-sysroot-native/usr/bin/python3-native:/home/zumi/Project/Yocto_4_9_88/nxp-yocto/sources/poky/scripts:/home/zumi/Project/Yocto_4_9_88/nxp-yocto/bld-xwayland/tmp/work/imx6slevk-poky-linux-gnueabi/gstreamer1.0-plugins-base/1.12.2-r0/recipe-sysroot-native/usr/bin/arm-poky-linux-gnueabi:/home/zumi/Project/Yocto_4_9_88/nxp-yocto/bld-xwayland/tmp/work/imx6slevk-poky-linux-gnueabi/gstreamer1.0-plugins-base/1.12.2-r0/recipe-sysroot/usr/bin/crossscripts:/home/zumi/Project/Yocto_4_9_88/nxp-yocto/bld-xwayland/tmp/work/imx6slevk-poky-linux-gnueabi/gstreamer1.0-plugins-base/1.12.2-r0/recipe-sysroot-native/usr/sbin:/home/zumi/Project/Yocto_4_9_88/nxp-yocto/bld-xwayland/tmp/work/imx6slevk-poky-linux-gnueabi/gstreamer1.0-plugins-base/1.12.2-r0/recipe-sysroot-native/usr/bin:/home/zumi/Project/Yocto_4_9_88/nxp-yocto/bld-xwayland/tmp/work/imx6slevk-poky-linux-gnueabi/gstreamer1.0-plugins-base/1.12.2-r0/recipe-sysroot-native/sbin:/home/zumi/Project/Yocto_4_9_88/nxp-yocto/bld-xwayland/tmp/work/imx6slevk-poky-linux-gnueabi/gstreamer1.0-plugins-base/1.12.2-r0/recipe-sysroot-native/bin:/home/zumi/Project/Yocto_4_9_88/nxp-yocto/sources/poky/bitbake/bin:/home/zumi/Project/Yocto_4_9_88/nxp-yocto/bld-xwayland/tmp/hosttools"; export HOME="/home/zumi"; git -c core.fsyncobjectfiles=0 submodule update --init --recursive failed with exit code 1, output:
Submodule 'common' (https://anongit.freedesktop.org/git/gstreamer/common.git) registered for path 'common'

Cloning into 'common'...
fatal: unable to access 'https://anongit.freedesktop.org/git/gstreamer/common.git/': Failed to connect to anongit.freedesktop.org port 443: Network is unreachable
Clone of 'https://anongit.freedesktop.org/git/gstreamer/common.git' into submodule path 'common' failed

ERROR: gstreamer1.0-plugins-base-1.12.2-r0 do_fetch: Fetcher failure for URL: 'gitsm://source.codeaurora.org/external/imx/gst-plugins-base.git;protocol=https;branch=MM_04.03.05_1804_L4.9.88_MX7ULP_GA'. Unable to fetch URL from any source.
ERROR: gstreamer1.0-plugins-base-1.12.2-r0 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /home/zumi/Project/Yocto_4_9_88/nxp-yocto/bld-xwayland/tmp/work/imx6slevk-poky-linux-gnueabi/gstreamer1.0-plugins-base/1.12.2-r0/temp/log.do_fetch.27898
ERROR: Task (/home/zumi/Project/Yocto_4_9_88/nxp-yocto/sources/poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.12.2.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1 tasks of which 0 didn't need to be rerun and 1 failed.

Please provide me the guidance.

#imx6sl#yocto imx‌ 

タグ(2)
0 件の賞賛
3 返答(返信)

2,210件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Karthikeyan,

Please erase everything about yocto and reinstall again, the project exist that the reason of the error.

regards

0 件の賞賛

2,210件の閲覧回数
karthikeyanraju
Contributor III

Hi Bio_TICFSL,

I m using ubuntu 16.04 LTS.

Following the below document for 4.9.88 yocto version and building imx6slevk xwayland image.

Is my way is right ?

Document Number: IMXLXYOCTOUG
Rev. L4.9.88_2.0.0-ga, 05/2018

0 件の賞賛

2,210件の閲覧回数
karthikeyanraju
Contributor III

Hi,

I was using 14.04 LTS , I have changed my machine to 16.04 LTS because there is no support for 14.04 machine.

Today I m facing another erroe as follows.

Initialising tasks: 100% |######################################################################################################| Time: 0:00:12
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: lttng-modules-2.10.5-r0 do_package: lttng-modules: no modules were created; this may be due to CONFIG_TRACEPOINTS not being enabled in your kernel.
WARNING: python3-iniparse-native-0.4-r0 do_fetch: Failed to fetch URL https://files.pythonhosted.org/packages/source/i/iniparse/iniparse-0.4.tar.gz, attempting MIRRORS if available
ERROR: weston-3.0.0-r0 do_prepare_recipe_sysroot: Error executing a python function in exec_python_func() autogenerated:
The stack trace of python calls that resulted in this exception/failure was:
File: 'exec_python_func() autogenerated', lineno: 2, function: <module>
     0001:
 *** 0002:extend_recipe_sysroot(d)
     0003:
File: '/home/zumi/Project/yocto_4.9_release/sources/poky/meta/classes/staging.bbclass', lineno: 565, function: extend_recipe_sysroot
     0561:                    dest = newmanifest[l]
     0562:                    if l.endswith("/"):
     0563:                        staging_copydir(l, targetdir, dest, seendirs)
     0564:                        continue
 *** 0565:                    staging_copyfile(l, targetdir, dest, postinsts, seendirs)
     0566:
     0567:    bb.note("Installed into sysroot: %s" % str(msg_adding))
     0568:    bb.note("Skipping as already exists in sysroot: %s" % str(msg_exists))
     0569:
File: '/home/zumi/Project/yocto_4.9_release/sources/poky/meta/classes/staging.bbclass', lineno: 151, function: staging_copyfile
     0147:        os.symlink(linkto, dest)
     0148:        #bb.warn(c)
     0149:    else:
     0150:        try:
 *** 0151:            os.link(c, dest)
     0152:        except OSError as err:
     0153:            if err.errno == errno.EXDEV:
     0154:                bb.utils.copyfile(c, dest)
     0155:            else:
Exception: FileExistsError: [Errno 17] File exists: '/home/zumi/Project/yocto_4.9_release/bld-xwayland/tmp/sysroots-components/cortexa9hf-neon/systemd/sysroot-providers/systemd' -> '/home/zumi/Project/yocto_4.9_release/bld-xwayland/tmp/sysroots/imx6slevk/sysroot-providers/systemd'
ERROR: weston-3.0.0-r0 do_prepare_recipe_sysroot: Function failed: extend_recipe_sysroot
ERROR: Logfile of failure stored in: /home/zumi/Project/yocto_4.9_release/bld-xwayland/tmp/work/cortexa9hf-neon-mx6sl-poky-linux-gnueabi/weston/3.0.0-r0/temp/log.do_prepare_recipe_sysroot.30156
ERROR: Task (/home/zumi/Project/yocto_4.9_release/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics/wayland/weston_3.0.0.bb:do_prepare_recipe_sysroot) failed with exit code '1'
Waiting for 2 running tasks to finish:
Need support for this.
0 件の賞賛