Graphics on iMX6Solo using mainline kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Graphics on iMX6Solo using mainline kernel

1,297 Views
mod42
Contributor III

Hi

Is it possible to use accelerated graphics on iMX6Solo with the current mainline (3.19 RC) kernel? If yes then what have to be done to get it working?

Regards

Matthias

Labels (3)
0 Kudos
Reply
2 Replies

1,058 Views
LaurenPost
NXP Employee
NXP Employee

Starting with our recent 3.10.53-1.1.0 GA release that just came out it is possible to mix and match kernels starting this release (but with graphics from previous releases like 3.10.17).  We separated out the  graphics kernel driver into a loadable module.  Now we made this change so customers in future would have ability to mix and match graphics releases with other kernels (only starting with 3.10.53) but did not consider it being used for community kernels.  However it should  work - we've just not tried it.

0 Kudos
Reply

1,058 Views
mod42
Contributor III

Thanks for your answer. And sorry for asking a dumb question again: Where can I download that release? I can only find something called L3.10.17_1.0.0_IMX6QDLS_BUNDLE

0 Kudos
Reply