Gpu performance on imx7ulp device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Gpu performance on imx7ulp device

10,841 次查看
ravicalm
Contributor I

Hi all,

I am using the imx7ulp board for my project . I am using yoct os . I have to know the gpu performance while rendering or capturing the image. I observed while rendering the image , the logs present in the code was used it under os/linux/drivers/gpu/drm/etnaviv that means my gpu using the ethnaviv driver instead of galcore driver. could you please help me in meausring the performance of gpu which is using the ethnaviv driver for rendering. 

标签 (1)
0 项奖励
回复
9 回复数

10,804 次查看
ravicalm
Contributor I

I have the following info

Operating System: Poky (Yocto Project Reference Distro) 2.7.1 (warrior)

Kernel: Linux 4.14.98

uname -a Linux fly 4.14.98

#1 SMP PREEMPT Mon Jul 10 16:01:38 UTC 2023

armv7l GNU/Linux build/yocto/poky/meta-yocto-bsp/conf : file content

# We have a conf and classes directory, add to

BBPATH BBPATH .= ":${LAYERDIR}" # We have recipes-* directories,

add to BBFILES BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \ ${LAYERDIR}/recipes-*/*/*.bbappend"

BBFILE_COLLECTIONS += "yoctobsp" BBFILE_PATTERN_yoctobsp = "^${LAYERDIR}/"

BBFILE_PRIORITY_yoctobsp = "5"

LAYERVERSION_yoctobsp = "4"

LAYERSERIES_COMPAT_yoctobsp = "warrior"

0 项奖励
回复

10,840 次查看
ravicalm
Contributor I
@Dhruvit/@chivara could you please respond i hope u guys have given info on gputop tool/gpuinfo.sh script which will internally uses galcore but in my case while rendering I am seeing the logs in ethnaviv module instead of galcore so could you please share any tool or point to the code where we can see the percentage of gpu used .
0 项奖励
回复

10,838 次查看
ravicalm
Contributor I

is ethanaviv driver runs/helps  on gpu or helps the gpu for rendering could you please confirm?

is ethanviv driver will run on cpu?

could you please clarify me about the ethnaviv driver

0 项奖励
回复

10,806 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which version BSP are you using, we can help confirm.

0 项奖励
回复

10,797 次查看
ravicalm
Contributor I
I have the following info

Operating System: Poky (Yocto Project Reference Distro) 2.7.1 (warrior)

Kernel: Linux 4.14.98

uname -a Linux fly 4.14.98

#1 SMP PREEMPT Mon Jul 10 16:01:38 UTC 2023

armv7l GNU/Linux build/yocto/poky/meta-yocto-bsp/conf : file content

# We have a conf and classes directory, add to

BBPATH BBPATH .= ":${LAYERDIR}" # We have recipes-* directories,

add to BBFILES BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \ ${LAYERDIR}/recipes-*/*/*.bbappend"

BBFILE_COLLECTIONS += "yoctobsp" BBFILE_PATTERN_yoctobsp = "^${LAYERDIR}/"

BBFILE_PRIORITY_yoctobsp = "5"

LAYERVERSION_yoctobsp = "4"

LAYERSERIES_COMPAT_yoctobsp = "warrior"
0 项奖励
回复

10,633 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

You are using the ethnaviv driver not the GPU driver we using, so we do not have test the performance for this driver.

If you want to use the GPU of NXP, you can modify in the Menuconfig.

You can refer to our i.MX_Graphics_User's_Guide.pdf document.

In menu configuration enable the following module for the GPU driver:
CONFIG_MXC_GPU_VIV is a configuration option for GPU driver. In the menuconfig this option is available under Device Drivers
> MXC support drivers > MXC Vivante GPU support > MXC Vivante GPU support.
On the screen displayed, select Configure the kernel, select Device Drivers > MXC support drivers > MXC Vivante GPU support
> MXC Vivante GPU support, and then exit. When the next screen appears, select the following options to enable the GPU driver:
• Package list > imx-gpu-viv
• This package provides proprietary binary libraries, and test code built from the GPU for framebuffer

0 项奖励
回复

10,613 次查看
ravicalm
Contributor I

@Rita_Wang I am not able to found MXC support drivers under the menuconfig I will give the screen shot of my menuconfig

0 项奖励
回复

10,565 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

You can following our i.MX Graphics User’s Guide document.

0 项奖励
回复

10,755 次查看
ravicalm
Contributor I
@Rita_Wang reply??
0 项奖励
回复