Gpu demo crashed under iMX6_SDK with iMX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gpu demo crashed under iMX6_SDK with iMX6DL

1,939 Views
laufei
Contributor III

Hello, Freescale

I am using the iMX6_SDK to test the GPU demo based on the iMX6DL version.

By the way, I run this gpu demo successfully on the iMX6Dual version.

the following log shows the issue:

------------log-----------------------------

**************************************************************************

    Platform SDK (1.1) for MX6SDL TO1.1 

    Build: Sep 26 2014, 11:12:19

**************************************************************************

Running GPU test, please connect the Hannstar LVDS panel to the LVDS0

GPU test running, press any key to exit.

Oops, data abort occurred!

Registers at point of exception:

cpsr = nzCvqeAift Supervisor (0x20000113)

r0 = 0x00000002    r8 =  0x00000000

r1 = 0x002000e4    r9 =  0x00000000

r2 = 0x002000e4    r10 = 0x00000000

r3 = 0x00f000e4    r11 = 0x10404248

r4 = 0xdeadfeed    r12 = 0x1040424c

r5 = 0x100752a0    sp =  0x10404224

r6 = 0x00000000    lr =  0x1006e11c

r7 = 0x00000094    pc =  0x10068af4

dfsr = 0x00000008

dfar = 0x00f000e4

Access type: read

Fault status: 0x8

-------------------------------------------------------------------

Can you help me check this issue?

Thank you very much.

Labels (1)
0 Kudos
Reply
6 Replies

1,817 Views
Yuri
NXP Employee
NXP Employee

This is "normal behaviour" of the SDK tests after exit,

assuming the GPU test is itself working.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,817 Views
laufei
Contributor III

Hi, Muhin

Thank you for your quickly reply.

When running the gpu demo, I didn't press anykey to exit the gpu demo, and the LVDS screen also shows mess info.

While using the iMX6Dual version, it's ok for showing the rolling ball.

I am thinking the SDK for gpu demo is not tested for iMX6DL version?

Thanks.

Best Regards

Fe la

0 Kudos
Reply

1,817 Views
Yuri
NXP Employee
NXP Employee

  The i.MX6 DQ and S/DL have different 3D hardware (Vivante GC2000 and GC880), therefore 

please try to rebuild the GPU test for target = mx6sdl.

~Yuri.

0 Kudos
Reply

1,817 Views
laufei
Contributor III

Hi, Yuri

yes, I seleted the target is mx6sdl to build the GPU demo test other than  it can't print the console output.

--------------------------------------------------------------------------------------------

make target=mx6sdl board=smart_device boardrev=c

--------------------------------------------------------------------------------------------

can you help me check the sdk codes for this part?

Thanks.

0 Kudos
Reply

1,817 Views
Yuri
NXP Employee
NXP Employee

Sorry, I cannot get information, if the GPU demo was tested for i.MX6 S/DL.


~Yuri.

0 Kudos
Reply

1,817 Views
Yuri
NXP Employee
NXP Employee

  I do not have the i.MX6DL on hands to check the problem, sorry.

Let me try to know if app team tested the i.MX6DL.
I expect it may take a time.

~Yuri.

0 Kudos
Reply