Google play service on sabre-sdp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Google play service on sabre-sdp

ソリューションへジャンプ
1,496件の閲覧回数
JHY
Contributor IV

How can I install google play service on sabre-sdp?

ラベル(1)
タグ(2)
1 解決策
1,092件の閲覧回数
art
NXP Employee
NXP Employee

Please note that only the base Android operating system (including some basic applications) is open-source software, whereas most Android devices ship with a substantial amount of proprietary software, such as Google Mobile Services, which includes applications such as Google Play Store, Google Search, and Google Play Services – a software layer that provides APIs for the integration with Google-provided services, among others. These applications must be licensed from Google by device makers, and can only be shipped on devices which meet its compatibility guidelines and other requirements.

So, you should have the manufacturer's license from Google to be able to implement the Google Play service on your platform. You can contact Google for more details:

https://source.android.com/compatibility/

https://source.android.com/compatibility/contact-us.html


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,093件の閲覧回数
art
NXP Employee
NXP Employee

Please note that only the base Android operating system (including some basic applications) is open-source software, whereas most Android devices ship with a substantial amount of proprietary software, such as Google Mobile Services, which includes applications such as Google Play Store, Google Search, and Google Play Services – a software layer that provides APIs for the integration with Google-provided services, among others. These applications must be licensed from Google by device makers, and can only be shipped on devices which meet its compatibility guidelines and other requirements.

So, you should have the manufacturer's license from Google to be able to implement the Google Play service on your platform. You can contact Google for more details:

https://source.android.com/compatibility/

https://source.android.com/compatibility/contact-us.html


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信