Dear all.
I'm working with a Nitrogen6X which has a i.MX6 chip.
I'm trying to configure the global timer to be the timer for the scheduler of the RTOS that I'm porting to the board.
I can configure it the way I want but the sticky interrupt flag is always at 1 after I serve the interrupt.
The ARM Information Center states that "The event flag is cleared when written to 1." What does this mean?
I have tried to write 0 directly to the register that holds the flag (Global Timer Interrupt Status Register), I tried to write 1, I tried to disable the interrupts of the timer and the compare functionality, but nothing seems to work.
Thanks in advance
Tiago Duarte
已解决! 转到解答。
Solution: turn of the compare flag and write 1 to the Global Timer Interrupt Status Register. Then turn on again the compare flag.