Github website crashes using chromium browser for BSP 6.1.55

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Github website crashes using chromium browser for BSP 6.1.55

2,545 次查看
hankwang
Contributor V

Hi ,

       We add chromium browser in the BSP 6.1.55_2.2.0 and test github website. The Chromium browser will be shutting down . We tested on i.MX8M Plus Evaluate Board.  Can anyone help?

标记 (1)
0 项奖励
回复
9 回复数

2,519 次查看
hankwang
Contributor V

Hi , Thanks for your reply. We follow the i.MX Yocto Project User Guide Rev LF6.1.55_2.2.0 document to build the bsp.

The instructions are as follows :

$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-mickledore -m imx-6.1.55-2.2.0.xml
$ repo sync

$ DISTRO=fsl-imx-wayland MACHINE=imx8mpevk source imx-setup-release.sh -b build-wayland

Add Chromium Browser on Wayland

Add this CORE_IMAGE_EXTRA_INSTALL += "chromium-ozone-wayland" in imx8mpevk.conf. 

The path is at " /meta-imx/meta-bsp/conf/machine"

$ bitbake imx-image-full

When the bsp image is installed on the 8MP EVK board, you can follow the instructions to launch the chromium browser.

$ chromium --no-sandbox

 

 

 

 

0 项奖励
回复

2,514 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Have a try to add this CORE_IMAGE_EXTRA_INSTALL += "chromium-ozone-wayland" to conf/local.conf

 

Regards

Harvey

0 项奖励
回复

2,510 次查看
hankwang
Contributor V

Yes we did. So we can use chromium browser to work on 8M Plus EVK Board.

This feature command is added just to add chromium browser to the bsp image. It can be in local.conf or imx8mpevk.conf.

0 项奖励
回复

2,521 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

Can you share how you build the BSP 6.1.55_2.2.0 with corresponding steps?

 

Regards

Harvey

0 项奖励
回复

2,448 次查看
hankwang
Contributor V
Hello, I have replied to you. Can you replicate the same problem?
0 项奖励
回复

2,430 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Yes, the same problem here, unfortunately, we don't provide support and test the patches.

 

Regards

Harvey

0 项奖励
回复

2,427 次查看
hankwang
Contributor V
May we know, would you raise this issue with the RD?
0 项奖励
回复

2,328 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @hankwang 

Gor reply from R&D as below.

For customer's case, users may need to add "--disable-gpu" to the command. 

show as following:

"chromium --no-sandbox --disable-gpu "

Disables GPU hardware acceleration. If software renderer is not in place, then the GPU process won't launch. You can reference the following ling about Chromium's issue and usage:

1.Headless: make --disable-gpu flag unnecessary - chromium

2.Chromium - ArchWiki (archlinux.org)

3. List of Chromium Command Line Switches « Peter Beverloo

 

Regards

Harvey

0 项奖励
回复

2,423 次查看
Harvey021
NXP TechSupport
NXP TechSupport

I've raised a case to internal team, please wait, will let you know if any update. 

 

Regards

Harvey

0 项奖励
回复