Getting started with wireless connectivity on i.MX6 Duallite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Getting started with wireless connectivity on i.MX6 Duallite

620 次查看
karthik_mohan
Contributor II

I have a i.MX6 Duallite Rev A (MCIMX6U5DVM10AC) with Wandboard as the carrier board Rev D. The SoM has AP6335 module for WiFI+ Bluetooth 4.0+ FM support. I wanted to user wireless, but can get the interface up and running.

I am using the kernel (tn-imx_4.9.88_2.0.0_ga-test) cloned from from TechNexion's github repository.

I have enabled the following Kernel configurations while building the kernel.

CONFIG_BCMDHD = y

CONFIG_BCMDHD_SDIO = y

CONFIG_BCMDHD_FW_PATH = "/lib/firmware/brcm/brcmfmac4339-sdio.bin"

CONFIG_BCMDHD_NVRAM_PATH = "/lib/firmware/brcm/brcmfmac4339-sdio.txt"

 

I have configured the device tree (imx6dl-wandboard.dtb) to include the required changes.

 

 regulators {
 compatible = "simple-bus";
 #address-cells = <0x1>;
 #size-cells = <0x0>;

         wlreg_on:fixedregulator@100 {
                     compatible = "regulator-fixed";
                     regulator-min-microvolt = <5000000>;
                     regulator-max-microvolt = <5000000>;
                     regulator-name = "wlreg_on";
                     enable-active-high;
        };

};

 bcmdhd_wlan_0: bcmdhd_wlan@0 {
 compatible = "android, bcmdhd_wlan";
 wlreg_on-supply = <&wlreg_on>;
 };

 I am using Ubuntu 16.04 LTS.

 

Can anyone help me out on how to bring up the wlan interface?

 

标记 (2)
0 项奖励
回复
0 回复数