Getting started with i.MX 8M Nano

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting started with i.MX 8M Nano

Jump to solution
1,622 Views
dibyajyoti
Contributor II

I am planning to use the new 8M Nano module in my design for a smart meter product. What would be the best place to start development?

Labels (2)
Tags (1)
0 Kudos
1 Solution
6 Replies
1,437 Views
dibyajyoti
Contributor II

Thank you very much for your continued support. 

0 Kudos
1,437 Views
dibyajyoti
Contributor II

Thank you very much for the links diegoadrian and romitchatterjee Thank You ‌!

Can you point me to some links where I can buy the evk?

Thanks.

0 Kudos
1,437 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

You can find more information on the following web-page. Just go under the buy option part.

i.MX 8M Nano Evaluation Kit | NXP 

Hope this information could be useful to you.

Best regards,

Diego.

0 Kudos
1,437 Views
romitchatterjee
Contributor V

You should get started by getting an evk first (i.MX 8M Nano Evaluation Kit | NXP ). You can find the getting started guide here: i.MX 8M Nano EVK Board Getting Started Guide | NXP .

0 Kudos
1,437 Views
diegoadrian
NXP Employee
NXP Employee

Hello, 

If you are willing to use the i.MX8MN. I suggest you use our Linux BSP. You could find more information on the following web-page.
One can find most of the information under the supporting information part.
 
Furthermore, you can start using our SDK to implement the M4 cortex in all the real-time processing applications that your product needs. You can find them in the following web-page:
You just need to select the desired board and the packages that you want to add.
 
Hope this information can be useful to you.
Best regards,
Diego.
0 Kudos