Getting kernel panic in imx8mplus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Getting kernel panic in imx8mplus

1,580 次查看
srinivas_123
Contributor III

I am using imx 8mplus lpddr4 evk and custom board of imx8mplus . i  build yocto BSP of 6.6.3 version.

i buid the two images  separately for evk and custom board.

in evk image , I changed the RAM size from 6gb to 1gb , frequency I kept default(4000mts)

in custom board image , I changed the RAM size to 6gb to 1 gb , frequency I configured 2400MTS

on evk , I flashed the my image , it is working fine .

on custom board , it is showing kernel panic .

 

Thanks & Regards

Srinivas

0 项奖励
回复
1 回复

1,492 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Can you also try 2400MTS on EVK?

Table 3.  IMX8MPlus LPDDR4 Typical Frequency Point

DDR Data Rate/MTS

DDR frequency/MHZ

DRAM_PLL_FDIV_CTL0

4000

2000

0xFA031

3200

1600

0xC8031

2400

1200

0x12C032

1600

800

0x190033

1066

533

0x10A033

667

334

0x14E034

0 项奖励
回复