Hi,
we are using i.MX6 #imx6 dualplus/6quadplus Custom Board.
In that we are observing little flickering once booting up. after pSplash Screen comes,
when starting X11 Server little flickering observed #display flicker x11 #xorg-server
when debugged we have observed various observation,
Below are the Observations.
Ob 1 : while debugging "/etc/init.d/xserver-nodm" in this script file X11 server is starting >>>>>>>> echo "Starting Xserver" >>>>>>>> . /etc/X11/xserver-common >>>>>>>> xinit /etc/X11/Xsession -- `which $XSERVER` $ARGS >/var/log/Xsession.log 2>&1 after commenting above script board boots completely without any flickering but not moving from psplash screen to Yocto desktop after that once enabled, Psplash screen goes then LCD flickers start for 2 - 4 seconds then going to Yocto Linux Home page. #splash_screen
Ob2 : Further debugging in X11 folder under the linux file system we got know one script called "/etc/X11/xorg.conf" in this script #xserver-xorg-video-imx-viv
Section "Device"
Identifier "i.MX Accelerated Framebuffer Device"
Driver "vivante"
Option "fbdev" "/dev/fb0"
Option "vivante_fbdev" "/dev/fb0"
Option "HWcursor" "false"
Option "mode_settings" "false"
EndSection
Section "ServerFlags"
Option "BlankTime" "0"
Option "StandbyTime" "0"
Option "SuspendTime" "0"
Option "OffTime" "0"
EndSection
>>>>>> however mode_settings in false but still why X11 starts flickering
Ob 3 : After exploring into in-depth we have got some answered query from
NXP community below are the link,
https://community.nxp.com/thread/328618
in above link same observation has got to one user also they have solved but unfortunately they are using Old Yocto kernel.
We are using Linux 4.1.15 Linux Kernel BSP. #linux kernel 4.1.15 #linux bsp #linux-source #linux device tree #freescale bsp