Getting PCM audio data through ESAI port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Getting PCM audio data through ESAI port

2,101 次查看
JHY
Contributor IV

Is that possible to get PCM audio data through EASI port?

I want to connect bluetooth module and i.MX6, so audio channel for them is needed.

It may be necessary drivers for PCM because my system is based on Linux 3.10.

Best regards.

标签 (2)
标记 (3)
3 回复数

1,806 次查看
art
NXP Employee
NXP Employee

Of course, it is possible to get the PCM audio through the ESAI port on i.MX6 platform under Linux 3.10.xx control. For more information, please refer to the ALSA chapter of your Linux Reference Manual document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,806 次查看
sumit8915
Contributor III

Hi Artur,

 

    We have a custom Designed Board based on i.mx6D, Where the SLIC IC, LE9641 (Supporting PCM +SPI) is connected to the AUDMUX interface and the SPI interface of the i.mx6D respectively.

We are able to communicate with the SLIC IC trough SPI interface, but i m not getting CLOCK from the AUDMUX fro the PCM interface.

Could you please suggest anything on this?

Thanks

Sumit

1,806 次查看
JHY
Contributor IV

Thank you for your help.

Is there a reference schematics or pin-mux guide for PCM mode?

0 项奖励
回复