Hi Guys,
I'm enabling HABv4 secure-boot on imx8mm. As usual, need an SPL hab block to create the CSF descriptor file e.g
Blocks = 0x7e0fd0 0x1a000 0x2e600 "flash.bin"
It works totally fine when we do all the signing steps manually. But to automate the signing process with Yocto there is an issue. It is possible that the build gets complete from caches, without generating build logs.
So, is there any way to get this spl hab block offset value directly from the boot image? or similar, like we can print fit block values?
$ make SOC=<SoC Name> print_fit_hab