I recently created a linux kernel for arm using yocto with this repository: GitHub - Freescale/fsl-community-bsp-base: BSP base files perfoming the following steps (I didn't modified the conf provided by default):
- repo https://github.com/Freescale/fsl-community-bsp-base.git
- repo sync
- MACHINE=imx6qdlsabresd DISTRO=fslc-x11 source setup-environment build
- bitbake meta-choolchain
And I got the a the kernel 4.15.7
So far it is fine for me but I can't find the dcic driver files.
Do I need to build the yocto distro using other parameters or the dcic should be added with patches?
Thanks for any help!
Solved! Go to Solution.
Hi Marcos,
On NXP BSP the DCIC driver is available in the directory: <Yocto_BuildDir>/linux/drivers/video/fbdev/mxc/.
On the screen displayed, select Configure the Kernel, When the next screen appears, select the
following options as build-in status to enable this module
Device Drivers -> Graphics support -> MXC DCIC
Regards
Hi Marcos,
On NXP BSP the DCIC driver is available in the directory: <Yocto_BuildDir>/linux/drivers/video/fbdev/mxc/.
On the screen displayed, select Configure the Kernel, When the next screen appears, select the
following options as build-in status to enable this module
Device Drivers -> Graphics support -> MXC DCIC
Regards