Generation of u-boot image for I.MX8QM Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generation of u-boot image for I.MX8QM Board

338 Views
mallibeerala
Contributor III

I am trying to generate u-boot image for I.MX8QM board(imx-5.15.32-2.0.0), by using following procedure but proper u-boot image is not generating, but u-boot  image available in NXP server is working properly.

Currently I am following below procedure for generating u-boot image.

bitbake u-boot-imx -c clean -f

bitbake -c devshell u-boot-imx

make imx8m_mek_defconfig (at git folder) --> Is this configuration is correct or not, please confirm.

bitbake u-boot-imx -c fetch

bitbake u-boot-imx -c compile

bitbake u-boot-imx -c deploy

At finally I am getting u-boot-sd-2022.04-r0.bin, u-boot-spl.bin-sd-2022.04-r0 and u-boot-imx-initial-env-imx8qmmek-sd-2022.04-r0 images but these images are not working.

Please help us to create proper u-boot for I.MX8QM board.

Mallikarjuna B,

Thanks & Regards.

0 Kudos
1 Reply

322 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

For i.MX8 chips, it uses the flash.bin image, which is actually the boot image container set, can include SCFW, SECO FW, M4 image, ATF image, U-Boot image, and SPL image.

To create this binary please refer to the Linux documentation, i.MX_Linux_Users_Guide.pdf
4.5.13 How to build imx-boot image by using imx-mkimage

Best regards,
Aldo.

0 Kudos