I am working on pwm audio driver, i got some pwm driver from below link:
GitHub - Glowforge/kernel-module-imx-pwm-audio: i.MX6 PWM audio driver
Please look at this driver once from above..............................
| code from driver... "sdma-params" passing from device tree |
|---|
| /* Read SDMA channel number and load address */ if (of_property_read_u32_array(pdev->dev.of_node, "sdma-params", sdma_params, ARRAY_SIZE(sdma_params)) == 0) { // if (of_property_read_u32_array(pdev->dev.of_node, NULL, // NULL,0)) { self->sdma_ch_num = sdma_params[0]; self->sdma_script_origin = sdma_params[1]; } else { dev_err(&pdev->dev, "sdma-params property not specified"); goto failed_sdma_init; } |
while passing the parameters of sdma(channel No. and address of sdma script load address ) in devicetree the board is not booting(its booting till bootloader), is because of channel number and address?
| Devicetree |
|---|
| &pwm3 { comaptible = "glowforge,imx-pwm-audio"; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_pwm3>; enable-gpio = <&gpio1 4 0>; timer = <0x10>; sdma-params = <0x19 0xdc0>; status = "okay"; |
Please suggest me how to pass these parameters through devicetree and also give some examples to understand it.
Thanks & Regards
Ganesh K
Hi Ganesh
official nxp bsps do not support sdma pwm as this requires new sdma script.
Above link is custom driver with custom sdma script, not supported by nxp, seems
it is working with releases described below (L3.14.28)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------