Generate BCLK from the IMX6 for a tas2562 as slave mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generate BCLK from the IMX6 for a tas2562 as slave mode

1,682 Views
henri_pineau
Contributor I

Hi,

For several days I try to generate a BCLK clock from the IMX6 for a TAS2562.

The tas2562 is in slave mode, he has is own MCLK clock internally.

The TAS2562 need a BCLK at 3MHz and WCLK at 48KHz

Before, I used a TAS2552 with an external MCLK. Is there a relation with the external MCLK and the BCLK generated by the IMX ?

My imx-tas2562.c (dai_init function) :

2020-04-21_09h27_41.png

Is the function have an impact on the BCLK generation ?

Could you explain me how to generate my BCLK from my IMX without external MCLK ?

Best regards,

PINEAU Henri

Labels (1)
0 Kudos
Reply
7 Replies

1,570 Views
henri_pineau
Contributor I

Hi,

Actually, I have a BCLK and WCLK. The WCLK have a 48KHz frequency and the BCLK the same.

Normally WCLK = n*BCLK. I don't now where my BCLK comes from ! I'm sure it is internal because there is no MCLK on the TAS2562. And I can't change the frequency.

Is it clearer ?

Best regards

Henri

0 Kudos
Reply

1,570 Views
igorpadykov
NXP Employee
NXP Employee

Hi Henri

please look at sgtl5000 connections and software designed by

boundary devices, TAS2562 should have similar connections

as on p.7 schematic https://boundarydevices.com/sabre_lite-revD.pdf 

Best regards
igor

0 Kudos
Reply

1,570 Views
henri_pineau
Contributor I

Hi Igor,

I have the similar connections and the hardware is ok. The mclk of the TAS2562 is internal. There are just DIN, DOUT, BCLK and WLCK are provided by the IMX. So I don't have mclk generate from the IMX. There is a link between mclk and the bclk ?

Best regards,

Henri

0 Kudos
Reply

1,570 Views
igorpadykov
NXP Employee
NXP Employee

Hi Henri

>There is a link between mclk and the bclk ?

for i.MX6DQ - no.

for TAS2562 suggest to check its datasheet or ask

its vendor - https://e2e.ti.com/support/amplifiers/f/14 

Best regards
igor

0 Kudos
Reply

1,570 Views
henri_pineau
Contributor I

Hi Igor,

The tas2562 is a slave module, so the bclk must be generated by the IMX.

My DT for the TAS2562 :

2020-04-22_14h16_01.png

2020-04-22_14h15_34.png

Best regards,

Henri

0 Kudos
Reply

1,570 Views
igorpadykov
NXP Employee
NXP Employee

Hi Henri

you can try any suggested boundarydevices audio examples,

for example using sgtl5000 and you will see bclk.

Audio amplifier example

https://community.nxp.com/thread/384918 

Best regards
igor

0 Kudos
Reply

1,570 Views
igorpadykov
NXP Employee
NXP Employee

Hi PINEAU

>Could you explain me how to generate my BCLK from my IMX

one can look at sect.61.8.4.1 SSI Clock and Frame Sync Generation

i.MX 6Dual/6Quad Applications Processor Reference Manual

also one can look at audio overview from boundary devices

https://boundarydevices.com/audio-output-selection-under-linux-on-i-mx6/ 

https://boundarydevices.com/tag/audio/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply