Galcore does not create a device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Galcore does not create a device

ソリューションへジャンプ
3,198件の閲覧回数
MicMoba
Contributor V

Hi,

I need some support around the GPU topic of the iMX8MP.

After I switched from Kernel 5.15.52 to Kernel 6.6.23 my LVDS display did not work as expect.

I recognized that the galcore kernel module did not create a device (/dev/galcore).

How can I found out why the device is not create? I tried to remove the module and insert again but this works without error messages. I searched in dmesg and journalctl but also with no success.

 

So what possibilities do I have to get more information? 

タグ(4)
0 件の賞賛
返信
1 解決策
3,062件の閲覧回数
MicMoba
Contributor V

Hi I found out that I miss to enable the mix_gpu_ml node in the devicetree.

After I add the lines

&mix_gpu_ml {
	status = "okay";
};

and reboot I have a /dev/galcore device. And now I am also able to start weston

元の投稿で解決策を見る

8 返答(返信)
3,104件の閲覧回数
MicMoba
Contributor V

I checked the following things:

$ strings /usr/lib/libGAL.so | grep VERSION
  $VERSION$6.4.11:745085:bc7b6a2a0f$

$ strings /usr/lib/modules/6.6.23-v6.6.23-2.0.0-phy-ge2011246/updates/galcore.ko | grep VERSION
  $VERSION$6.4.11:745085$

$ldconfig -p | grep libGAL.so
  libGAL.so (libc6,AArch64) => /lib/libGAL.so

So the Galcore firmware (libGAL.so) and the kernel module (galcore.ko) have the same version. I can see the galcore with lsmod command.

I have a /dev/dri/card0 device but no /dev/galcore device

Which possibilities do I have to do further checks? How is the connection between LVDS and Galcore?

 

0 件の賞賛
返信
3,096件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You have galcore in your system and it's ready to use, you just need to send the graphics to lvds, make sure your display is lvds in uboot.

Regards

0 件の賞賛
返信
3,088件の閲覧回数
MicMoba
Contributor V

That's a point I will check.

You mean it is not necessary to have a device called /dev/galcore ? I thought this is mantandory for a iMX8 system with Vivante GPU.

This is a part of weston 12 output:

 

 

[12:26:48.568] libseat: session control granted
[12:26:48.571] using /dev/dri/card0
[12:26:48.571] DRM: supports atomic modesetting
[12:26:48.571] DRM: does not support GBM modifiers
[12:26:48.571] DRM: does not support async page flipping
[12:26:48.571] DRM: supports picture aspect ratio
[12:26:48.571] Loading module '/usr/lib/libweston-12/gl-renderer.so'
[     1] Failed to open device: No such file or directory, Try again...
[     2] Failed to open device: No such file or directory, Try again...
[     3] Failed to open device: No such file or directory, Try again...
[     4] Failed to open device: No such file or directory, Try again...
[     5] _OpenDevice(1031): FATAL: Failed to open device, errno=No such file or directory.
[     6] Failed to open device: No such file or directory, Try again...
[     7] Failed to open device: No such file or directory, Try again...
[     8] Failed to open device: No such file or directory, Try again...
[     9] Failed to open device: No such file or directory, Try again...
[    10] _OpenDevice(1031): FATAL: Failed to open device, errno=No such file or directory.
[12:26:56.585] [seatd/client.c:471] Client disconnected

 

 

I thought the "Failed to open device" messages were from a missing /dev/galcore device. How can I get more information about the missing file or directory?

タグ(2)
0 件の賞賛
返信
3,063件の閲覧回数
MicMoba
Contributor V

Hi I found out that I miss to enable the mix_gpu_ml node in the devicetree.

After I add the lines

&mix_gpu_ml {
	status = "okay";
};

and reboot I have a /dev/galcore device. And now I am also able to start weston

3,117件の閲覧回数
mgordon
Contributor I

I'm seeing the same issue with 5.4. galcore driver is loaded, but no /dev/galcore device.  Nothing in either dmesg or journalctl. Any suggestions?

 

0 件の賞賛
返信
3,168件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Send us you dmesg log file is not possible not building the galcore in 6.6.23.

regards

 

0 件の賞賛
返信
3,133件の閲覧回数
MicMoba
Contributor V

Can you tell me how the procedure with the vivante galcore firmare is?

The firmware is a binary blob. The kernel module loads the firmware and initialize the GPU. Is the firmware part of the kernel module (galcore.ko) or should there a .bin file in the /lib/firmware folder which is load?

0 件の賞賛
返信
3,165件の閲覧回数
MicMoba
Contributor V

Hi,

you will find the dmesg output in the attachment

0 件の賞賛
返信