GT911 IC Not working in Kitkat iMX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GT911 IC Not working in Kitkat iMX6SL

867 Views
jansirani
Contributor III

Hai,

we have a custom board same as iMX6SLEVK design.

we want to integrate 5inch display which is having GT911 Touch IC.

Display is working properly.

we used this link  Re: [PATCH] Input: driver for the Goodix touchpanel — Linux Input and integrated the touch .

I2c is detecting and getevents also coming in the console, but still unable to lock the screen.

Thanks & Regards,

D.Jansirani

Labels (4)
0 Kudos
2 Replies

490 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jansi

one can test with ts_test, some useful links

https://community.nxp.com/message/447781?commentID=447781#comment-447781 

http://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/

http://boundarydevices.com/tweaking-froyo-for-nitrogen-part-1-touch-support/

had you tested i2c lines with oscilloscope

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

490 Views
jansirani
Contributor III

Hai igorpadykov

we monitored the i2c scl and sda lines using oscilloscope.

when we touch the screen i2c signals are pulsing but there is no response from the display side.

0 Kudos