Hi, I'm using a CM-FX6 board ... having issues trying to run GStreamer.
I'm trying to get analog tv in via ADV7180 ... what could be the problem here?
root@cm-debian:/# gst-launch tvsrc ! autovideosink
MFW_GST_tvsrc_PLUGIN 3.0.7 build on Jul 31 2013 18:18:05.
Setting pipeline to PAUSED ...
MFW_GST_V4LSINK_PLUGIN 3.0.7 build on Apr 18 2013 23:22:23.
sensor chip is adv7180_decoderERROR: unrecognized std! ffffff (PAL=ff, NTSC=b000
should set the input to 1
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
ERROR: from element /GstPipeline:pipeline0/MFWGstTVSRC:mfwgsttvsrc0: Internal data flow error.
Additional debug info:
gstbasesrc.c(2582): gst_base_src_loop (): /GstPipeline:pipeline0/MFWGstTVSRC:mfwgsttvsrc0:
streaming task paused, reason error (-5)
Execution ended after 10005284338 ns.
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Total rendered:0
[--->FINALIZE v4l_sink
Freeing pipeline ...
root@cm-debian:/#
When I do gst-inspect :
root@cm-debian:/# rm ~/.gstreamer-0.10/registry*
root@cm-debian:/# gst-inspect > inspectlog
(gst-plugin-scanner:19754): GStreamer-WARNING **: Failed to load plugin '/usr/lib/gstreamer-0.10/libgstffmpegscale.so': libswscale.so.2: cannot opy
(gst-plugin-scanner:19754): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed
(gst-plugin-scanner:19754): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed
root@cm-debian:/# find / -name libswscale.so.2
root@cm-debian:/#
The following may be helpful.
GStreamer Pipeline issue for SII9135/ADV7180 CSI input
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------