Hi All.
I try build system i.MX53 ( qsb-board) with GPU.
I build BSP with Yocto - Rocko , Sumo , Thud , Warrior , Zeus.
I see GPU does not work.
After that I build kernel 5.4 with Yocto - Rocko , Sumo , Thud , Warrior , Zeus.
GPU does not work.
In addition, I see , we have problem with X11.
I see xorg.conf file ,
Section "Device"
Identifier "i.MX Accelerated Framebuffer Device"
Driver "imx"
Option "fbdev" "/dev/fb0"
# This option only recognized when "mxc_epdc_fb" frame buffer driver in
# use. Values are "RGB565" (default, 16-bit RGB), "Y8" (8-bit gray),
# and "Y8INV" (8-bit gray inverted).
Option "FormatEPDC" "Y8INV"
EndSection
, we have problem.
If we change : Driver "imx" to Driver "fbdev" , Xort is working.
Section "Device"
Identifier "i.MX Accelerated Framebuffer Device"
Driver "fbdev"
Option "fbdev" "/dev/fb0"
# This option only recognized when "mxc_epdc_fb" frame buffer driver in
# use. Values are "RGB565" (default, 16-bit RGB), "Y8" (8-bit gray),
# and "Y8INV" (8-bit gray inverted).
Option "FormatEPDC" "Y8INV"
EndSection
I think no work GPU accelerator.
Maybe someone launched the GPU on i.MX53.
Best regards.