Hi,
We have a custom platform based on SabreSD imx6q reference running Lollipop L5.1.1_2.0.0 GA (LMY47V) [kernel:3.14.38-138123]
We have been seeing a problem wherein the gpu and the display would just hang randomly.
System remains in the same state unless rebooted.
i have figured out that for some reason using chrome, with random events is the fastest way to reproduce this problem.
[Running "monkey --throttle 100 -p com.android.chrome 1000000" infinitely]
Tried with Android 5.1.1 2.0.0-ga-rc4 on sabre and i am able to reproduce the problem.
It takes some time before the screen is unresponsive. Android shell is responsive underneath.
Attached are the video and logcat for the problem happening on sabre board
Is this a known issue or could you help us in fixing this ?
Have this posted here already. Was advised to post on this forum.
HISTORY:
Already tried sabresd_6dq-eng 5.1.1 2.1.0-ga-rc3 and problem happens on this build also.
Tried galcore.powerManagement=0, causes the problem every time on system resume after suspend.
Tried NXP provided patch to disable GPU's power management feature. Issue still happens
We have seen the problem randomly also, while not using chrome.
Testing it on chrome package with monkey is helping us to reproduce this more often.
[Running "monkey --throttle 100 -p com.android.chrome 1000000" infinitely]
The version of chrome that is reproducing the problem for us is version 57.0.2987.132.
This version does not have the "Merge Tab" setting.
Other source to get it from: The Open GApps Project
On our platform we have seen signatures like:
03-20 13:49:40.478 156 156 I kernel : <6>[36394.351361] fence timeout on [d01dda00] after 3000ms03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] objs:03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] --------------03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] viv timeline viv_sync03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] pt signaled@2623.89748603-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] pt signaled@33633.69666903-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] pt signaled@33644.29413903-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] pt signaled@33644.88948303-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] pt active03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] pt active03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] pt active03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552]03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] viv timeline viv_sync03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552]03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] viv timeline viv_sync03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552]03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] fences:03-20 13:49:40.478 156 156 W kernel : <4>[36394.351552] --------------03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] [00000000] viv sync_fence-62573: signaled03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] viv timeline_pt signaled@2623.89748603-20 13:49:40.479 156 156 W kernel : <4>[36394.351645]03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] [00000000] viv sync_fence-64567: signaled03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] viv timeline_pt signaled@33633.69666903-20 13:49:40.479 156 156 W kernel : <4>[36394.351645]03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] [00000000] viv sync_fence-64577: signaled03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] viv timeline_pt signaled@33644.29413903-20 13:49:40.479 156 156 W kernel : <4>[36394.351645]03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] [00000000] viv sync_fence-64622: signaled03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] viv timeline_pt signaled@33644.88948303-20 13:49:40.479 156 156 W kernel : <4>[36394.351645]03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] [00000000] viv sync_fence-64624: active03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] viv timeline_pt active03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645]03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] [00000000] viv sync_fence-64625: active03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] viv timeline_pt active03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645]03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] [00000000] viv sync_fence-64626: active03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645] viv timeline_pt active03-20 13:49:40.479 156 156 W kernel : <4>[36394.351645]03-20 13:49:40.480 163 176 E Fence : Throttling EGL Production: fence 36 didn't signal in 3000 ms
03-20 13:50:29.885 156 156 W kernel : <4>[36443.761373] [galcore]: GPU[0] hang, automatic recovery.03-20 13:50:29.885 156 156 W kernel : <4>[36443.761450] [galcore]: recovery done03-20 13:50:34.880 163 933 W SurfaceFlinger: setTransactionState timed out!03-20 13:50:34.884 163 176 W SurfaceFlinger: setTransactionState timed out!
Original Attachment has been moved to: sabreLog.txt.zip
Hi neeraj
please try Demo Image on Sabre SD board
Best regards
igor
Hi Igor,
If you missed it in the earlier comment, and also could not determine it from the bugreport
- We tried the demo bsp for Android N - 7.1.1/1.0.0-ga-rc10 on SABRE SD board and it hangs.
Is NXP not able to reproduce the problem ?
We have been seeing the same problem on different sabre boards and each of our device based on Sabre platform also.
Also, it would be helpful to mention again here that, it was already posted here and was being actively worked by NXP support team. So the related NXP team has already seen the problem on their end.
Thanks
Hello!
Did you find any solution to this problem? We have similar problems with GPU after resuming from suspend. We've also asked NXP with no result (you've already posted our thread link - IMX AXI BUS ERROR, GPU hang )
Hi neeraj
seems there is some misunderstanding.
If you already submitted issue on that link, this means
that imx application team is already working on that issue
(mentioned link is internal confidential and closed for external customers).
I would suggest to continue work on that issue with contacts
from that link. Sorry I have not access to them.
Best regards
igor
Hi neeraj
L3.14.38 is very old kernel and since then lot of gpu errata were fixed,
please try latest described on
i.MX 6 / i.MX 7 Series Software and Development Tool|NXP
Fixed errata are described in Release Notes document from documentation package
which can be found on that link
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Moving to newer versions of lollipop is not an option for our platform.
Its a huge effort. We need to fix this on Lollipop 5.1.1.
Do you have any updates or patches for Lollipop 5.1.1 ?
Thanks
Hi neeraj
please check available patches on
i.MX 6 / i.MX 7 Series Software and Development Tool|NXP
Best regards
igor