GPU driver upgrade for old LinuxBSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPU driver upgrade for old LinuxBSP

1,711 次查看
torus1000
Contributor V

Hi

2 monthes ago, latest BSP(L.3.14.52) was released and some GPU bugs were fixed.

Please see "i.MX Linux® Release Notes".

  * GPU driver upgraded to Vivante v5.0.11p7.4.

  * There were 3 kinds of kernel panic bugs.

According to the NOTE** below, driver can be upgraded.

So I want to try upgrading GPU driver (galcore) with old BSP(L3.10.17).

Have ever someone tried to backport/applied those GPU patches to old BSP?

  https://github.com/Freescale/kernel-module-imx-gpu-viv

Thanks.

p113 of  " i.MX Linux® Reference Manual"

13.1.1.3 Source Code Structure

Table below lists GPU driver kernel module source structure:

<Yocto_BuildDir>/linux/drivers/mxc/gpu-viv

  Table 13-1. GPU Driver Files

FileDescription
Kconfig Kbuild configKernel configure file and makefile
hal/kernel/archHardware-specific driver code for GC2000, GC880, GC400T, and GC320
hal/kernel/archvgHardware-specific driver code for GC355
hal/kernelKernel mode HAL driver
hal/os/linux/kernelOS layer HAL driver

 

NOTE**

If you replace the whole content in this directory, the GPU

kernel driver can be upgraded.

标签 (2)
0 项奖励
回复
1 回复

1,088 次查看
art
NXP Employee
NXP Employee

It seems not to be possible to backport the GPU drivers to earlier kernels, since the GPU hardware-specific code is provided in pre-compiled binary form by the GPU cores vendor.


Have a great day,
Artur

0 项奖励
回复