Hi,
I'm using GPT1 to capture data from an IC circuit.
Interrupt is triggering on rise and fall edges (kGPT_InputOperation_BothEdge) and everything works fine.
My question is what I cad do to even capture data signal levels at interrupt event i.e. "low or high"?
I have gone through chapters 12.1.5.1 to 12.1.5.10 but no of the registers contains that information.
Document Number: IMX8MMRM
Rev. 3, 11/2020
Pin used: IOMUXC_SAI3_RXFS_GPT1_CAPTURE1
Best regards,
Adde
已解决! 转到解答。
>How can I determine if interrupt has occurred on rising or falling edge.
sorry there is no way for that. In general one can reconfigure pin as gpio and read its state
in interrupt service routine.
Best regards
igor
Hi Igor,
But IMn is a configure bit.
This can be used to determine how transition on the input pin has been "configured".
For example wit "GPT_GetInputOperationMode" function.
In my configuration event is trigger on both rising and falling edge.
How can I determine if interrupt has occurred on rising or falling edge.
Best regards,
Adde
>How can I determine if interrupt has occurred on rising or falling edge.
sorry there is no way for that. In general one can reconfigure pin as gpio and read its state
in interrupt service routine.
Best regards
igor
He Adde
>what I cad do to even capture data signal levels at interrupt event i.e. "low or high"?
only available options are described in sect.12.1.5.1 GPT Control Register (GPTx_CR)
i.MX 8M Mini Applications Processor Reference Manual
The IMn bit field determines the transition on the input pin (for Input capture channel n), which will trigger a
capture event.
00 capture disabled
01 capture on rising edge only
10 capture on falling edge only
11 capture on both edges
Best regards
igor