GPS not working in Linux 3.14.52 and SABRESDP DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPS not working in Linux 3.14.52 and SABRESDP DL

1,486 Views
misbahk
Contributor I

Hi All,

I am using SABRESDP i.MX6 Duel lite board and linux 3.14.52

The GPS is connected to uart 3. I did the pin mux configuration in the boot loader and enabled the UART 3 driver in the device tree as :

Called in the bootlaoder late init function :

static void gps_setup(void)

{

        printf(" #### Starting GPS setup #### \n");

        /* EIM_DA00 - GPS_PWREN */

        imx_iomux_v3_setup_pad(MX6_PAD_EIM_DA0__GPIO3_IO00 |

                                MUX_PAD_CTRL(SPI_PAD_CTRL));

        /* Set as input */

        gpio_direction_output(IMX_GPIO_NR(3, 0),1);

        gpio_set_value(IMX_GPIO_NR(3, 0), 1);

        /* EIM_DA18 - GPS_PPS */

        imx_iomux_v3_setup_pad(MX6_PAD_EIM_D18__GPIO3_IO18 |

                                MUX_PAD_CTRL(UART_PAD_CTRL));

        /* Set as input */

        gpio_direction_input(IMX_GPIO_NR(3, 18));

        /* EIM_EB0 - GPS_RESET */

        imx_iomux_v3_setup_pad(MX6_PAD_EIM_EB0__GPIO2_IO28 |

                                MUX_PAD_CTRL(SPI_PAD_CTRL));

        /* Set as input */

        gpio_direction_output(IMX_GPIO_NR(2, 28),1);

        gpio_set_value(IMX_GPIO_NR(2, 28), 1);

        /* EIM_D24 - uart_tx */

        imx_iomux_v3_setup_pad(MX6_PAD_EIM_D24__UART3_TX_DATA |

                                MUX_PAD_CTRL(UART_PAD_CTRL));

        /* EIM_D25 - uart_rx */

        imx_iomux_v3_setup_pad(MX6_PAD_EIM_D25__UART3_RX_DATA |

                                MUX_PAD_CTRL(UART_PAD_CTRL));

        // Reset GPS

        printf(" Reset the GPS here \n");

        mdelay(1000);

        gpio_set_value(IMX_GPIO_NR(2, 28), 0);

        mdelay(1000);

        gpio_set_value(IMX_GPIO_NR(2, 28), 1);

        printf(" Reset of gps done \n");

}

I enabled the uart3 in the imx6dl-sabresd.dts file and made the vgen1 to generate 1.5 v

checked with the oscilloscope and make sure that all supply voltages for the GPS module, including the 3.15V VCC voltage on the pin 11, 1.5V V_BCKP voltage on the pin 5 and 3.15V antenna supply voltage on the RF connector are in place.

Then, during initial power-up, cycle (assert and then de-assert back) the GPS_RESET_B signal for at least 1s in the bootloader.

There is nothing i could see on the uart port 3 when i do the following :

cat /dev/ttymxc2

echo "0xAA 0x6A" > /dev/ttymxc2

cat /dev/ttymcx2

Please guide me to use GPS "AH1613" using linux over SABRESDP board.

--- Misbah

0 Kudos
Reply
1 Reply

875 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Please check the UART pin configuration in the dts file.

It is possible that the UART pins are configured by other node.

/Alejandro  

0 Kudos
Reply