Hi Friend
Gps module with a compatible bsp for tablet i.mx535.
Apart from the gm22 AR1520A
You know?
I can not find the gm22 on mouser and findchipd.com?
Part numbers for the 3g module on tablets sabre you know?
If possible, you give numbers?
Alternative models You know?
For wifi / bt is also athors Part Number to buy it You know?
huawei 820 u to do this right?
Hi FRARZIN
supported chips are described in Linux Manual
(mx53_sabre_tablet_linux.pdf) included in
and i.MX_Android_R10.x_Release_Note.html included in
IMX5X_R10_31_ANDROID_DOCSBUNDLE
such as 3g HuaWei EM750M/E180/E220/E770M (HSPA/WCDMA/GPRS).
For new modules (not mentioned in these documents) you will have to add
support (driver for new module).
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
TANKS for answer
for Gps module with a compatible bsp for tablet i.mx535.
Apart from the gm22 AR1520A
You know?
Hi FRARZIN
BSP is written for specific chips, which
are used on Freescale reference boards.
For other chips one needs to add driver for them.
Best regards
chip